show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
What conditions do you have to comply with when configuring ET 200S modules?
Part number:

Configuration Notes:
With the ET 200S, the number of pluggable modules depends on the header module, the module width and the length of the configuration and parameterization messages.

IM 151-1
 
  BASIC
6ES7151-1CA00-0AB0
ST
6ES7151-1AA05-0AB0
ST  FO
6ES7151-1AB05-0AB0
HF
6ES7151-1BA02-0AB0
Bus length1) max. 2m max. 2m max. 2m max. 2m
Max. number of operable modules2) 12 63 63 63
Parameter data length3) 198 bytes No limit on SIMATIC S7,
otherwise 244 bytes5)
No limit on SIMATIC S7,
otherwise 244 bytes5)
No limit on SIMATIC S7,
otherwise 244 bytes5)
I/O address area4) 88 I/O bytes 244 I/O bytes 244 I/O bytes 244 I/O bytes

IM 151-1 COMPACT
 
  32DI STANDARD
6ES7151-1CA00-1BL0
16DI/16DO STANDARD
6ES7151-1CA00-3BL0
Bus length1) Not applicable Not applicable
Max. number of operable modules2) 12 12
Parameter data length3) 218 bytes 244 bytes
I/O address area4) 100 I/O bytes 100 I/O bytes

IM 151-3
 
  PN ST
6ES7151-3AA23-0AB0
PN FO
6ES7151-3BB23-0AB0
PN HF
6ES7151-3BA23-0AB0
PN HS
6ES7151-3BA60-0AB0
Bus length1) max. 2m max. 2m max. 2m max. 0.5m
Max. number of operable modules2) 63 63 63 32
Parameter data length3) No limit No limit No limit No limit
I/O address area4) 256 I/O bytes 256 I/O bytes 256 I/O bytes 180 I/O bytes

Interface module with integrated CPU
 
 

IM 151-7
6ES7151-7AA20-0AB0
6ES7151-7AB00-0AB0
6ES7151-7FA20-0AB0

IM 151-8 PN/DP
6ES7151-8AB00-0AB0
6ES7151-8FB00-0AB0  

Bus length1) max. 2m max. 2m
Max. number of operable modules2) 63 63
Parameter data length3) 244 bytes -
I/O address area4) 244 I/O bytes -

Notes:
1)
For example, a digital or analog I/O module has a width of 15mm, a fail-safe module a width of 30mm and a DS motor starter a width of 45mm.

2)
The maximum number of operable modules stands for all modules that can be plugged between an interface module (IM) and the terminating module.

3)
Every module (including the interface and power modules) needs a parameterization message. The length of the parameterization message differs for the different modules. You can find out how long the parameterization message for a particular module is in the manual for the "ET 200S Distributed I/O System" in Entry ID 1144348. The values given in the "Parameter length" row in Table 1 above must not exceed the sum for the entire ET 200S row.
In the case of PROFINET IO, the parameter length is not relevant for the maximum configuration of the station.

4)
Most modules assign additional addresses in the I/O address area. Depending on the module used, input or output addresses or also input and output addresses can be assigned by a module. The number of addresses assigned depends on the type of the module. The maximum value specified (in Table 1, "I/O address area" row) must not exceed the sum for the entire ET 200S subrack.
If the I/O address area specified for the IM151-7 CPU is used as I slave, it serves as transfer memory with the higher-level master.
Altogether, the IM151-7 CPU and the IM158-2 PN/DP can address an address area of 2048 bytes. Thus, when using the IM151-7 CPU or the IM158-2 PN/DP, a maximum of 16336 digital I/O channels or 1021 analog I/O channels can be addressed.
If you use the IM151-7 CPU or the IM158-2 PN/DP as DP master, then you need the DP master interface 6ES7138-4HA00-0AB0 in addition.

5)
With the configuration as from STEP 7V5.4, you have the option of operating the IM 151-1 ST as from 6ES7151-1AA05-0AB0 in the DPV1 mode with more than 244 bytes of parameter data. Configuration with the GSD does not provide this option.
With the configuration as from STEP 7V5.4, you have the option of operating the IM151-1 FO as from 6ES7151-1AB05-0AB0 in the DPV1 mode with more than 244 bytes of parameter data. Configuration with the GSD does not provide this option.
With the configuration as from STEP 7V5.3 SP3, you have the option of operating the IM151-1 HF as from 6ES7151-1BA02-0AB0 in the DPV1 mode with more than 244 bytes of parameter data. Configuration with the GSD does not provide this option.

More information on IM151-7 is available in the manual "ET 200S IM 151-7 CPU Interface Module" in Entry ID: 12714722.

More information on IM151-8 is available in the manual "Interface Module IM151-8 PN/DP CPU" in Entry ID: 29738847.

Note:
Use the SIMATIC Selection Tool to configure your ET 200S station. This configurator guides you conveniently and simply through the configuration of an ET 200S station and supports you in selecting the various components and matching accessories.

The SIMATIC Selection Tool is in the configuration tool overview of the Industry Mall under Automation Technology.

Industry Mall

 Entry ID:21406019   Date:2010-03-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour