show the entry list
OS - WinCC -- Configuring Alarm Logging -- Configuring alarms and messages
How can you create operator inputs through user-specific actions in up to and including WinCC V6.0 SP4?
How do you display and operate alarms in Runtime?
What do you do if alarms are not displayed at Runtime?
How can you change the column width of the message blocks with the mouse in WinCC Alarm Control when configuring in the Graphics Designer or in Runtime?
Configuring the system block "PLC/CPU number" in messages
Why are measuring-point-specific messages not displayed in the faceplate (PCS 7 V4.x / V5.x)?
What can you do if no messages are displayed in the overview area of WinCC?
Generating a new time stamp despite identical operator messages
Triggering of the horn with messages that are blocked for specific users
Why are the time stamps of messages struck through or replaced by asterisks in PCS 7?
SIMATIC PCS 7 V5/V6 - non-acknowledgable messages on the message new page
What are the priorities for the display of faults, warnings etc. in the group display?
How can you have a block comment displayed in an operator message?
Why are operator messages shown only on the OS server and not on the OS client?
Why after upgrading from PCS 7 V6.0 SP2 to SP3 isn't the operator who acknowledges a message entered in the operator message?
Why doesn't the operator prompt flash in the group display?
Modification of the printing color in the tag logging
How can I make messages for a certain operator be displayed in WinCC Runtime but cannot be acknowledged?
How can you reconfigure the alarm acknowledgment behavior?
Why isn't the process message displayed in my PCS 7 project?
How do you suppress the process control group messages?
What is the meaning of the process control group messages created during OS compilation?
Which process control group messages are created in the OS?
OS - WinCC -- Working with projects -- Creating and editing projects
How do you use a monitor with a 1680x1050 pixel resolution with the OS project editor in WinCC?
Why is the "Import" function no longer available?
Configuration in SIMATIC PCS 7 V6 - OS-Project editor
How can you reconfigure the alarm acknowledgment behavior?
What should you do if the OS server project is taken online by mistake on the ES?
Modification of SIMATIC PCS 7 OS Project Type
How do you proceed when the package name is not correct in your project?
Error message when saving the Picture Tree Manager for cross-reference in SIMATIC PCS 7 V5.x
PCS 7 V6: Standard Layout instead of Server View Layout in WinCC RT
How can you reconfigure the alarm acknowledgment behavior?
Part number:

Message Acknowledgment

                        
                        

QUESTIONS:

 

Troubleshooting and Handling Instructions

T1 How can you set important system messages, like failure of the partner server in the case of loss of redundancy, to "requires acknowledgment"?
T2 How can a message be acknowledged automatically in the OS station?

Product and System Functions

P1 Why are messages that cannot be acknowledged displayed in the reloaded message list?

Go to description of changes: FAQ History

ANSWERS:

Answer T1
How can you set important system messages, like failure of the partner server in the case of loss of redundancy, to "requires acknowledgment"?

When you create an OS project, system messages are generated from the standard WinCC environment when the OS project editor is run. These are all assigned to the message class "System, need not be acknowledged". Individual messages, like failure of a redundant partner, might however be so important that they should be set to "requires acknowledgment". For this it is recommended to proceed as follows:
 
No. Procedure
1 Open the Alarm Logging Editor in the WinCC Explorer. Select the required single message and right-click on it to open the "Properties" (in the example Message 1012200 for failure of the partner server). Select the required properties (in the example the class, type and the option "single acknowledgment only").


Bild T1-01

2 Save the change with "OK". The changed messages are marked in color in the Alarm Logging Editor.


Bild T1-02

Warning:
A message of the class "System, requires acknowledgment" is not displayed in any of the standard message lists (new list, old list, outgoing list, operation list, control system list, chronicle list). A corresponding extended selection can also be made offline or online.

Note:
These changes are not deleted after a renewed OS compilation, not even if you select "Overall reset". The changes are also retained after running the OS project editor.
Only running the OS project editor with the setting "Complete configuration" resets all the changes. However, this setting must be made manually each time you call the OS project editor, so that you cannot reset changes by mistake.


Bild T1-03

Back to Questions 
 

Answer T2 
How can a message be acknowledged automatically in the OS station?

It is not possible to acknowledge a message automatically in the OS station.
Back to Questions 
 

Answer P1 
Why are messages that cannot be acknowledged displayed in the reloaded message list?

The reloaded message list contains messages that cannot be acknowledged. The message can only be acknowledged when it is generated again. 
The OS server actively fetches all the messages currently available from all the automation systems when Runtime is started and displays them (with crossed-out time stamp, because that is the time of the startup, but not the time of when the fault occurred).
If the property "Reload Message List After Power Failure" is selected in the Message archive, then the old contents of the message archive are also fetched from a buffer, which means that many entries are in duplicate. In a PCS 7 project the property "Reload Message List After Power Failure" should not be enabled at all. 
If this property is enabled, messages are reloaded and possibly also messages that might have already been acknowledged. The associated driver block in the PCS 7 AS cannot accept such a message , because it has already been acknowledged.

Furthermore, the entries below are to be found in "WinCC_Sys*.log" (sample message):
....,NRMS7PMC,CquitFreiSperr::CreateTelegram: for msg-number 874592975 unknown function dwNotify

You can avoid this state by making the following entry in the message archive:
 
No. Procedure
1 In the Alarm Logging under "Archive Configuration > Message archive" you deselect the property "Reload Message List After Power Failure".


Bild P1-01

Back to Questions 
 

FAQ History
Change Date
FAQ created.
FAQ 17298206 has been incorporated into the present FAQ and deleted as a separate FAQ.
April 7, 2005
Back to Questions 
 

 Entry ID:21378784   Date:2010-12-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour