show the entry list
Touch Panel / Operator Panel -- Product information -- Determining performance and quantity frameworks
Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?
What are the functional differences between the different SIMATIC panels?
What should you watch out with regard to licenses for WinCC flexible and panels?
Contrast on OP5/15/7/17
Data record loss after transfer of configuration to line OP
No standard project in WinCE devices
Slower reaction times than usual with OP7/17
Configuration of the OP 17 DP 12 with ProTool 2.xx or older version of ProTool
Hardware test on the TP27
Contrast on OP5/15/7/17
Part number:

QUESTION:
How do I set the?

ANSWER:
You have two options for setting the contrast on an OP5/15/7/17:

  • Direct setting
    1. Press the "Shift” key. The shift LED lights.
    2. Press the "+/-” key until you get the required level of contrast.
    3. Press the "Shift” key.
  • Standard image
    1. Select the standard image "System” -> "Languages”.
    2. Move the cursor to "Contrast”.
    3. Select the required contrast level by entering symbolic values (1 for the lowest contrast, 16 for the highest).

 Entry ID:213455   Date:1998-02-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour