show the entry list
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
Which can be connected directly to a panel?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Floppy disk drive on OP 15, OP 17 and C7-624
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Cable for loading the configuration onto OP/TP
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Cable for loading the configuration onto OP/TP
Part number:

QUESTION:
Which cable do I need to load the configuration onto an OP/TP?

ANSWER:
The following table shows which cable you must use to load the configuration onto an OP/TP.

k_ops_25.pdf (9034 Bytes)

 Entry ID:213289   Date:1998-01-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour