show the entry list
ProTool -- Working with projects -- Upgrading to new version
How do you migrate a ProTool project with SIMOTION CPU connection to a WinCC flexible project and SIMOTION SCOUT?
Which version of Image of the relevant operator panels can be used for the corresponding version of ProTool?
Converting old configurations to Runtime - Procedure for ProTool versions prior to V6.0
Open Pro Tool 1.x configuration with current software
Which device is a suitable replacement for an OP25?
What solution can be offered for a defective MP40/C36A?
What changes do you have to make in the configuration after replacing the OP/TP 25/35 by an OP/TP 27/37 in a connection with the SIMATIC S5 via PROFIBUS DP?
What changes are necessary when a WF470 is replaced by an MP270 Touch in an S5 controller?
Open Pro Tool 1.x configuration with current software
Part number:

QUESTION:
I want to open a configuration made with Pro Tool V1.x with a more recent Pro Tool software. What must I watch out for?

ANSWER:
A configuration made with Pro Tool version V2.0 or higher only has one PDB file.
If you have created a configuration with Pro Tool Version 1.x then an additional folder is created for the PDB file bearing the same name.
If you now open the configuration made with Pro Tool V1.x under, for example, Pro Tool Version 2.51, then the PDB and the folder with the same name must be available.

 Entry ID:213253   Date:1998-01-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour