show the entry list
What are the derating factors for 3TF Contactors at higher frequencies?
Part number:
QUESTION:
What are the derating factors for 3TF Contactors at higher frequencies?

ANSWER:
At frequencies equal or higher than 100 Hz the thermal load rating of switchgear is reduced. The reason for this is the so called ''skin effect'' at higher frequencies. This skin effect causes a current flow near the surface of a conductor and not through its full cross section. This effect is increasing with higher frequencies.
As a result the thermal load rating (continuous current) of contactors is reduced according to the following table:
--------------------------------------------------
- at 100 Hz: Ie AC-1 x 0,933
- at 200 Hz: Ie AC-1 x 0,871
- at 300 Hz: Ie AC-1 x 0,836
- at 400 Hz: Ie AC-1 x 0,812
--------------------------------------------------
Indicated are typical frequencies of practical applications.
Making- and breaking capacities are not reduced within this range.
The contactors are not suitable for frequencies higher than 1000 Hz since internal ferro-magnetic parts would be excessively heated by eddy currents.
 Entry ID:21267913   Date:2005-03-17 
I regard this article....as helpfulas not helpful                                 
related links
3TK5: What are the derating facto ...
3RT1: What are the derating facto ...
STEP 7 Professional V11.0 SP1
3UG: How do voltage monitoring re ...
SITRANS F Communication Module P ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour