QUESTION:
What is the purpose of 3SB1902-2AT, 3SB1902-2AU, 3SB1902-2AV
Support terminals? What are these products supposed to be used
for?
ANSWER:
3SB1902-2A. support terminals are designed like switching elements
for base mounting and can be fitted the same way inside 3SB18
enclosures. The function is that of a through-type terminal. These
support terminals facilitate the connection of potentials that
don't have to be switched. Another possibility is the connection of
diode elements.
Entry ID:21265296
Date:2005-03-17
This entry is available in the following languages: german