show the entry list
What surge suppressors can be used for magnet coils of 3TF8 Reversing Contactors?
Part number:
QUESTION:
What surge suppressors can be used for magnet coils of 3TF8 reversing contactors? Catalogues do not show any accessories.

ANSWER:
3TX7462-3J Varistors, as an example for Us = 230 V AC, can be used for the following reversing contactors:
- 3TF813
- 3TF8232
- 3TF8332
- 3TF863
Each contactor needs 2 of the above varistors. These varistors can be fixed with adhesive tape (already attached to each varistor) to the side wall of the contactor. This increases the width of each contactor by 13 mm.
 Entry ID:21264176   Date:2005-03-17 
I regard this article....as helpfulas not helpful                                 
related links
3UF5: What suppressors are requir ...
Reasons for contact welding in co ...
3RT19/3RT29 Accessories and Spare ...
What surge surge suppressors may ...
Surge suppressor for contactors 3 ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour