afficher la liste des articles
Getting started S7 project for SIWAREX FTC for belt scale (Step 7 Classic and TIA-Portal)
Nº de référence:


Description:

This getting started project shows an example of how a SIWAREX FTC can be integrated into a S7 system. It contains an S7 program with integration of SIWAREX FTC and message system. It also contains a WinCC flexible project with visualisation and handling of SIWAREX FTC as belt scale. A calibration is also possible.
 
Alternatively the project is available in Step 7 classic or TIA-Portal.
The project contains the languages English, German, French, Bulgarian, Russian and Chinese. 

Download of the software:

 FTC_GETTING_STARTED_BELT_SCALE_S7.zip (13414 KB) ( 13414 KB )

 FTC_GETTING_STARTED_BELT_SCALE_TIA.zip (7655 KB) ( 7655 KB )

 

 ID contribution:21063615   Date:2012-02-21 
Cette contribution...m´a aidéne m´a pas aidé                                 
related links
Getting Started S7 project for SI ...
Getting Started S7 Project for SI ...
Getting started S7 project for SI ...
Getting Started S7 Project for SI ...
Getting started S7 project for SI ...