show the entry list
WinCC -- Setting up development environments -- Parameterizing systems
What should you watch out for when running SIMATIC WinCC or SIMATIC PCS 7 with Microsoft SQL Server 2005 on PCs with multi-core or multiple processors?
How can you change the properties of the ToolTip text (font, font size, ...) in WinCC Runtime?
How can you set up auto logon for SIMATIC IPCs?
WinCC: settings in the pcANYWHERE
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows 2000
Symbol bars in the Graphics Designer can no longer be changed in size and location.
WinCC project information is not displayed correctly in the "WinCC Projects" folder in the Windows Explorer
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows NT
How do you use the SIMATIC shell to configure the terminal bus of a WinCC station?
Why are WinCC pictures shown incorrectly or with margins in Runtime when using TFT and flat screens?
Which settings must you make in the WinCC-Explorer under "Computer > Properties" on each computer locally?
How can you make "lost" buttons visible again in the toolbar of the WinCC Explorer or the WinCC Graphics Designer?
Why after changing the resolution or installing a second monitor on my computer is the Properties dialog not displayed in the Graphics Designer?
Why after changing the resolution or installing a second monitor on my computer is the Properties dialog not displayed in the Graphics Designer?
Part number:

Guidance:  
By changing the resolution the values of the X/Y position of the Properties dialog stored in the Registry might represent a value that cannot be displayed. In order to reset the values of the X/Y position of the Properties dialog to '0' and therefore make them visible again, you must run the Registry file contained in the Zip file below.

Propertiesdialog.zip ( 291 bytes )  

IMPORTANT
In general, no warranty can be given for direct changes in the Registry database, because this is entirely the responsibility of the user. In any case it is recommended to make a backup of the Registry before proceeding as described below. Furthermore, these settings are user-specific. This means that when there is a change of user, the Registry file has to be run again

 Entry ID:20780805   Date:2005-02-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour