show the entry list
PROFIBUS S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
Overall reset of CP443-5 Extended via NCM S7 PROFIBUS Diagnostics
CP443-5 Extended: Loading a configuration with high volume
Inconsistent system data when removing a PROFIBUS DP master system from the network
What should you watch out for when configuring a CP342-5 as DP master and why is it necessary to call the FC1 "DP_SEND" and FC2 "DP_RECV" functions in the user program of the CPU in order to transfer data?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
CP 342-5 -- How can you change the PROFIBUS address or the operating mode of the CP 342-5 in running operation?
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Connecting an S7-300 to a DP/PA-Link
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
Part number:

QUESTION:
What are the options for communication between a SIMOVERT and a PROFIBUS DP master?

ANSWER:
You have the following options for connecting a SIMOVERT as PROFIBUS DP slave to a PROFIBUS DP master:

1. Interfacing the slave to the integrated DP connection of an S7-300 CPU

When configuring your SIMOVERT slave in the HW Config you are requested to make a choice regarding the setpoint configuration. If you decide for the PPO type 5, then you have the choice between:
"PPO 5: 4 PKW | 4 + 4 + 2 PZD"
and
"PPO 5: 4 PKW | 10 PZD".
In both case the sum of all parameter and process data words is identical. There is however a difference in the communication process due to the different distribution of the consistent data areas.

If you select the configuration "PPO 5: 4 PKW | 4 + 4 + 2 PZD", then you must program the communication via three calls of the SFC 15 (DPWR_DAT) and SFC 14 (DPRD_DAT). You always use the SFC 15 and SFC14 when your data length is either 3 bytes exactly or greater than 4 bytes. Since in this case three data blocks of 8 bytes each and one data block of 4 bytes have been selected, it is necessary to have the three SFC calls. The fourth data block is 4 bytes long and can therefore be read directly.
Note: the format of the data length in the HW Config is of the "WORD" type.

If you select the configuration "PPO 5: 4 PKW | 10 PZD", then you only need two calls each of the SFC 15 (DPWR_DAT) and the SFC 14 (DPRD_DAT). One call for the parameter data block (PKW) and one for the process data block (PZD).

2. Using the CP342-5 as DP master

If you use the CP342-5 as DP master, it doesn't matter which setpoint configuration you choose. You can only use the functions FC1 (DP_SEND) and FC2 (DP_RECV). The system functions SFC14 and SFC15 are not available to you in this case.

Note: if you configure a SIMOVERT CBP together with a CP342-5, then the data block is two bytes longer than predefined in the HW Config (PKW+PZD). These two extra bytes are needed for diagnostics.

 

 Entry ID:2043578   Date:2000-04-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour