show the entry list
ET 200M (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Configuring SIPLUS extreme modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Which options are available for configuring the ET 200 stations?
Parameterization data of an analog module in an ET 200 are not transferred when using an external master
Configuring a power supply for an IMxxx in the ET200M
Configuring the Dummy Module => BF in ET200M
Parameterizing the ET200-M (IM153-x) only possible in hex code
The input values of an analog module in the ET 200M sporadically have the value zero
ET200-M with active backplane bus.
Configuring IM153-3 (ET200-M)
"Change of module during operation" parameter option on an ET 200 M
Operating ET200M as slave on master station CPU315-2DP
No startup of ET200M station when using blank slots
"Module change during operation" - Configuration and system requirements
Display of the "Parameter Assignment" tab for the configuration of modules
Output channels of SM 335 do not work
How do you calculate the times for the clock-synchronized operation of ET 200M?
Configuring SIPLUS extreme modules
Part number:

QUESTION:  
How can I configure SIPLUS extreme modules (order no.: 6AG1 ...) in STEP 7?

ANSWER:  
You have a SIPLUS extreme module for extreme environment conditions with order number 6AG1 ...  and would like to configure it with STEP 7.
For this you use the type based on this module with order number 6ES7 ... .

The following excerpt from the STEP 7 HW Config shows the configuration of an ET200M of SIPLUS extreme:
Slot 2: IM 153-1 with order number: 6AG1 153-1AA03-2XB0
Slot 4: SM 321 16DI with order number: 6AG1 321-1BH02-2AA0
Slot 5: SM 322 16DO with order number: 6AG1 322-1BH01-2AA0

Fig. 1: Sample configuration of an ET200M of SIPLUS extreme

Note
More information is available at www.siemens.com/siplus or in Entry ID: 18607092

If you were previously implementing SIMATIC Outdoor modules (6ES7 ...-...8.-....), you replace them in specific cases with SIPLUS extreme modules without having to reconfigure. For example, you can replace the following modules with an ET200M with order number 6AG1 153-1AA03-2XB0 (SIPLUS extreme) in a spare parts case without reconfiguration:

  • 6ES7 153-1AA03-0XB0
  • 6ES7 153-1AA83-0XB0
  • 6ES7 153-1AA02-0XB0
  • 6ES7 153-1AA82-0XB0

An overview of all the order numbers of the relevant SIMATIC, SIMATIC Outdoor and SIPLUS extreme modules is available in Entry ID: 17054970 
 

 Entry ID:19951150   Date:2011-12-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour