show the entry list
M44 - Board description files (BGB) for auto configuration
DESCRIPTION:
Board description files (BGB) for auto configuration.

BGB-/BGT files:
BGB and BGT files are used by the auto configuration program. They have the extension *.BGB or *.BGT and their position in the directory structure must be entered into SMPCNF:INI. Otherwise the program cannot be started.

BGB file
The BGB file is a description file for a SMP16 board. It is necessary for configuring this board and contains mandatory configuration settings as well as optional settings for the board. The BGB file influences the appearance of the auto configuration program by adjusting dialogue boxes for the different boards. This means that the BGB file determines which options for the respective board are enabled and which are not. The BGB file also contains information for enabling the various setting possibilities of the program. Every change in these settings by the user will corrupt the BGB file which will result in disabling of these setting possibilities in the main program. A BGB file must not be changed by the user!

BGT file
It contains the text shown in the dialogues. A BGT file can be edited by the user. The BGB- and BGT files of the same board must have the same name and also must not be renamed otherwise a program error will occur.

 

Download:

AMS-M44
 amsm44.exe ( 31 KB )

 Entry ID:1988702   Date:2001-04-05 
I regard this article....as helpfulas not helpful                                 
related links
COM167 - Board description files ...
COM225 - Board description files ...
COM291 - Board description files ...
COM595 - Board description files ...
CPU05x - Board description files ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour