show the entry list
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Connecting an S7-300 to a DP/PA-Link
S7-400 CPU 41x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How can time and date be acquired from a GPS signal?
How do you configure time synchronization?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can I procure the GSD files for my S7-400 CPUs?
How do you do a cold start with SIMATIC S7-400 CPUs version V4.0 and higher?
Why should you switch the operating mode of the CPU from Test to Process after commissioning the STEP 7 program?
How do you use or update process image partitions for S7-400 CPU modules during an interrupt OB?
Only up to 27 configured blocks are displayed
What should you watch out for with the "forcing inputs" function in the S7-400?
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Synchronizing time
How do you configure the SIMATIC S7-300 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode?
How do you configure time synchronization?
Where can you find information on the Siclock system?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?
How do you configure the SIMATIC S7-400 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode?
How do you configure a PC as NTP server?
Why can't you use the IEEE Standard 1588 for synchronizing SIMATIC controllers?
How do you configure time synchronization?
Part number:

Description:
In an automation network of multiple SIMATIC stations you have the option of synchronizing the clocks of all the CPUs. For this, you parameterize the clock of one CPU as the "master clock" and set the interval at which synchronization is to take place. You parameterize the CPUs to be synchronized as "slave clocks". You set the parameters via the CPU properties.


Fig. 01: Setting synchronization on a CPU 315-2DP as example

You can set synchronization separately:

  • in the PLC (i.e. internal)
  • on an MPI (i.e. external)
  • on an MFI (i.e. external via 2nd interface)

Detailed information on time synchronization is available from the following sources:

  • For S7-300 CPUs - the manual "S7-300 CPU 31xC and CPU 31x, Technical Data", "Interfaces" chapter, in Entry ID:12996906
  • For S7-400 CPUs - the manual "Automation System S7-400 CPU Specifications", "Time Synchronization" chapter, in Entry ID:23904550
  • For CP 343-1 - the device manual "Part B CP 343-1", "Time Synchronization" chapter, in Entry ID:24485272
  • For CP 443-1 - the device manual "Part B CP 443-1", "Time Synchronization" chapter, in Entry ID:27013386

Note:

  • A description of time synchronization via Industrial Ethernet with the SIMATIC procedure is available in Entry ID:18130164.
  • A description of time synchronization via PROFIBUS in the SIMATIC environment is available in Entry ID:17544115.
  • A description of time synchronization via MPI subnetwork in the SIMATIC environment is available in Entry ID:17521938.

 Entry ID:19866467   Date:2010-01-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour