show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
ET 200S (standard modules) -- Configuring and programming communication -- Using communication blocks
How in WinAC MP 2008 do you program data transfer with the ET200S 1SI module for the 4-byte or 8-byte communication type?
Which CPU can you operate as a PROFINET I device?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300 or S7-400 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange by means of the integrated PROFINET interface of a CPU?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
"Report System Errors" function can be used with ET 200S CPU from firmware version V2.1
Using the SFB75 (send alarm to the DP master) on an ET 200S CPU
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Basic Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you integrate an HMI operator panel into a local network?
What transfer options are available in the various operator panels?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
Part number:

Configuration Notes
Please note the following points if you wish to connect a SIMATIC HMI operator panel to an ET 200-CPU.

Properties of the ET 200-CPUs

  • ET 200S CPU
    The IM151-7 CPUs of ET 200S have an MPI/ DP interface.
    In the MPI subnetwork you can use the HMI operator panel to operate the ET 200S CPU via the integrated MPI interface.
    On the PROFIBUS DP the integrated DP interface of the ET 200S CPU can only be used as a DP slave. This means that in addition to the HMI operator panel you need a DP master (S7-300 CPU316-2DP, for example) that operates the IM 151-7 CPU as a DP slave.

    If the IM151-7 CPU is operated without DP master on the PROFIBUS DP, communication with the HMI operator works, but a bus error is displayed on the IM151-7 CPU.

    Note
    With the DP master module (order number 6ES7138-4HA00-0AB0), which you slot directly next to the ET 200S CPU, you can add a DP interface to the ET 200S, which is configured as DP master. With this master interface module it is then possible to operate the ET 200S without any other DP master on the PROFIBUS DP.

    Requirements
    In order to be able to use the DP interface on the master interface module you require a CPU, order number 6ES7151-7AA10-0AB0, and firmware version V2.1 or higher.

  • ET 200X CPU
    The BM147-1 CPUs of ET 200X have an MPI/ DP interface.
    In the MPI subnetwork you can use the HMI operator panel to operate the ET 200X CPU via the interface parameterized as MPI.
    On the PROFIBUS-DP the ET 200X CPU (BM 147-1) can only be used as a DP slave. This means that in addition to the HMI operator panel you need a DP master (S7-300 CPU316-2DP, for example) that operates the BM 147-1 as a DP slave.

    The BM147-2 CPUs of ET 200X have an MPI/ DP interface that can be parameterized as MPI or as a DP slave, and another DP master interface.
    In the MPI subnetwork you can use an HMI operator panel to operate the ET 200X CPU via the interface parameterized as MPI.
    On the PROFIBUS DP the ET 200X CPU BM 147-2 can operate on the one hand as a DP slave with an additional DP master (an S7-300 CPU 315-2DP, for example). On the other hand the BM147-2 CPU can also communicate as DP master with the HMI operator panel via the DP master interface.

Warning
The ET 200 CPU is configured in the SIMATIC Manager in a
SIMATIC S7-300 station.

Options for connecting an HMI operator panel to the ET 200 CPUs

Connecting the HMI operator panel via MPI to the ET 200 CPU
You can connect the HMI operator panel via MPI directly to an IM151 CPU or BM147 CPU.


Fig. 01

Setting in the STEP 7 Hardware Configuration
In the Properties dialog of the MPI/DP interface of the ET 200 CPU you set the type of interface to MPI and then connect the station to the MPI subnetwork.


Fig. 02

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the ET 200 CPU via MPI.


Fig. 03

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 04

Connecting the HMI operator panel via PROFIBUS DP to the ET 200 CPU

  1. Version: CPU 316-2DP as DP master, ET200 CPU as DP slave
  2. Version: ET200S CPU with DP master module
  1. Version: CPU 316-2DP as DP master, ET200 CPU as DP slave

The ET 200 CPU is operated as DP slave on the PROFIBUS DP subnetwork. This means that in addition to the HMI operator panel and the ET 200 CPU (IM151 CPU or BM147 CPU) you need a DP master (S7-300 CPU 316-2DP, for example) on the PROFIBUS DP subnetwork.


Fig. 05

Settings in the STEP 7 Hardware Configuration of the ET 200 CPU for supporting ALARM_S messages
In order for the ET 200 CPU to support the ALARM_S service, in the Properties of the DP interface of the IM151 CPU or BM147 CPU under Operating Mode you must enable the option Test, commissioning, routing.


Fig. 06

Settings in the STEP 7 Hardware Configuration of the S7-300 DP master
Once you have networked the ET 200 CPU with PROFIBUS DP, open the Hardware Configuration of the DP master station (CPU 316-2DP) and there you configure the ET 200 CPU as a DP slave.


Fig. 07

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the ET 200 CPU via PROFIBUS.


Fig. 08

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 09  

  1. Version: ET200S CPU with DP master module

The ET 200S is operated with the DP master interface module as DP master on the PROFIBUS DP. The HMI operator panel is connected to the master module via PROFIBUS.


Fig. 10

Settings in the STEP 7 Hardware Configuration
Network the DP master module of the ET 200S with a newly created PROFIBUS network.
The master interface module is located in the Hardware Catalog in the project tree from which you configured the IM151-7 CPU.


Fig. 11

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the DP master module of the ET 200 CPU via PROFIBUS.


Fig. 12

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 13

Connecting the HMI operator panel (MPI) via routing (CPU 316-2DP: DP Master) to the ET 200-CPU (DP-Slave)
THe ET 200 CPU (IM151 CPU or BM147 CPU) is operated as a DP slave on an S7-300 CPU 316-2DP (DP master). The HMI operator panel is connected to the S7-300 via MPI. Via routing (MPI <-> PROFIBUS DP) a connection is set up between the HMI operator panel and the ET 200 CPU.


Fig. 14

Settings in the STEP 7 Hardware Configuration of the ET 200 CPU for supporting ALARM_S messages
In order for the ET 200 CPU to support the ALARM_S service, in the Properties of the DP interface of the IM151 CPU or BM147 CPU under Operating Mode you must enable the option Test, commissioning, routing.


Fig. 15

Settings in the STEP 7 Hardware Configuration
Once you have networked the ET 200 CPU with PROFIBUS DP, open the Hardware Configuration of the DP master station (CPU 316-2DP) and there you configure the ET 200 CPU as a DP slave. The S7-300 station must also be networked with MPI.

 
Fig. 16

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the DP master module of the S7 -300 CPU (CPU 316-2DP) via MPI.


Fig. 17

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 18

Overview: HMI operator panels with ET 200 CPU
 

HMI operator panel

Communication
HMI operator panel
with
ET 200-CPU

Alarm_S messages supported

ProAgent
options package supported
KTP400 Basic - - -
KTP600 Basic X1) - -
KTP1000 Basic X1) - -
TP1500 Basic - - -
OP 73micro - - -
TP 170micro - - -
TP 177micro - - -
OP 77A X - -
OP 77B X X -
TP 170A X - -
TP 177A X - -
TP 170B X X -
TP 177B X X -
TP 177B 4" X X -
OP 170B X X -
OP 177B X X -
Mobile Panel 170 X X -
Mobile Panel 177 X X -
TP 270  X X X
TP 277  X X X
OP 270 X X X
OP 277 X X X
MP 177 X X X
MP 270 X X X
MP 270B X X X
MP 277 X X X
Mobile Panel 277 X X X
Mobile Panel 277 IWLAN - X X
Mobile Panel 277F IWLAN - X X
MP 370 X X X
MP 377 X X X
ProTool/Pro RT X X X
WinCC flexible RT X X X
1) Applies only for the DP version of this operator panel

Note
More information on configuring Alarm_S messages and the display on the operator panel is available in the Support Shop in Entry ID: 24013249.

 Entry ID:19835185   Date:2011-04-18 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour