show the entry list
S7-300 CPU 31x -- Configuring and programming communication -- Configuring PROFINETinterfaces
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
How do you reset the IP address and device name of an I device?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which CPU can you operate as a PROFINET I device?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
Can you implement an S7 317-2 PN/DP CPU instead of an S7 315-2 PN/DP CPU configured in iMap?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What can you do when communication errors occur sporadically with a PROFINET interface of the S7 300 CPU 31x-2 PN/DP?
From which library should you take the communications FBs?
What are the commonalities and differences between configured communication connections and the open Ethernet communication?
What are the differences when assigning the MAC address?
What can you do when communication errors occur sporadically with a PROFINET interface of the S7 300 CPU 31x-2 PN/DP?
Part number:

Instructions 
Please make sure that all the network components (switches) on the Ethernet (PROFINET) can always be operated with 100 Mbit/s full duplex. Do not use hub distributors, because these devices only support half-duplex mode.

 Entry ID:19809964   Date:2010-12-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour