show the entry list
WinCC SIMATIC Logon / AUA -- Product information -- Information on SIMATIC Logon / Advanced User Administrator
Using a chip card reader, how can a default user be logged on automatically while the chip card is pulled through?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of WinCC comply with FDA regulations?
How can you configure a chip card with SIMATIC Logon, with which you can log onto each local computer?
Why isn't the group selection dialog displayed any longer in WinCC V6.2 and higher?
How can you use the "GetSignature" function as of SIMATIC Logon V1.4?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
Why isn't the user currently logged on shown at Runtime?
How can you replace the Windows on-screen keyboard of SIMATIC Logon (from V1.4) with the ProTool keyboard so as not to reach the operating system during Runtime?
How can you verify a logged on user at runtime when using SIMATIC Logon (as from V1.3)?
How can you verify a logged on user at runtime when using SIMATIC Logon up to version V1.2 SP1?
How do you call the SIMATIC Logon dialog box by means of C-Script?
The WinCC Login Box appears instead of the Logon Box in WinCC Runtime.
How do you call the SIMATIC Logon dialog box by means of C-Script?
Part number:

Instructions:
The SIMATIC Logon interface is partly integrated into WinCC from WinCC V6.0 SP3 (or SIMATIC Logon V1.2). You can find further information about calling the SIMATIC Logon box either in the WinCC Online Help under:

  • "Release Notes > Notes on WinCC > Utilization of SIMATIC Logon",
  • "Working with WinCC > Setting Up User Administration > WinCC Options for the User Administrator > Option SIMATIC Logon",
  • or in the manual "SIMATIC Logon Electronic Signature", chapter 5.4.5, in Entry ID 34519648.   

The following instructions are valid for WinCC V6.0 SP1 and SP2 or SIMATIC Logon V1.1 SP2.

A SIMATIC Logon dialog box can be generated as follows:

  • Open the WinCC adapter via "Start > SIMATIC  > SIMATIC Logon > WinCC Adapter".

  • Click the "Adapt Project" button to enter the logon functions into the project's PDL files. Ensure that the WinCC project is open during the project adaptation. Click "Exit" to close the dialog box.


2

  • Go to the Graphics Designer and configure a button, for example, in a process picture; open a C-action under "Object Properties > Event > Button > Mouse > Mouse Click". Insert the following line (function) in the C-action:

    SIMATICLogon (* lpszPictureName );

    Then compile the action and save the change in the process picture.

Note:
The original function passlogin.fct was automatically changed during installation in previous versions of SIMATIC Logon - in this regard also read Entry ID 17543809.


 Entry ID:19552508   Date:2006-07-21 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour