show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
Part number:

QUESTION:  
What should you watch out for in the communications between a WinAC Basis/ WinAC RTX V4.0 and higher and a Windows-based operator panel configured with WinCC flexible 2004?

ANSWER:  
This entry provides instructions for configuring the link between the WinAC and a Windows-based operator panel configured with WinCC flexible 2004 via PROFIBUS.

Requirements:

  • MS Windows 2000 SP4 or MS Windows XP SP1
  • WinAC Basis V4.0 or RTX V4.0 and higher
  • WinCC flexible 2004
  • SIMATIC NET CD 11/2003
  • STEP 7 V5.3 SP1

Configuring the SIMATIC PC station for the WinAC

  • Open the SIMATIC Manager and create a new STEP 7 project.
  • Add a PC station via Insert > Station > SIMATIC PC Station.
  • Double-click Configuration to open the Hardware Configuration of the PC station.

Fig. 1: Adding a PC station to the STEP 7 project

  • Insert the relevant WinLC, for example WinLC Basis V4.1 (from the Hardware Catalog SIMATIC PC Station > Controller), into the rack of the PC station at Index 2.
  • Insert the relevant PROFIBUS CP, for example 5611, as IF module of the WinLC Basis and network this with PROFIBUS DP.

Warning:
WinLC RTX can be operated only with CP5613.

Fig. 2: Insert WinLC and CP5611

  • Save and compile the configuration.
  • Open the Station Configuration Editor on the WinAC computer.
  • The table in the Station Configuration Editor must match the assignment of the rack in the SIMATIC PC station.

Note:
The IF module is inserted in the Properties of the WinLC in the Station Configuration Editor. For this the CP must be in the configured mode.

  • In order to load the configuration into the WinAC the name of the PC station in the SIMATIC Manager must match the station name in the Station Configuration Editor on the WinAC computer.

Fig. 3: Station Configuration Editor

  • Also on the STEP 7 configuration PC you must change the PG/PC interface to the relevant type of transfer (here: S7ONLINE (STEP 7) --> CP5611 (PROFIBUS)).
  • Start the WinAC controller.
  • Load the STEP 7 project into the WinLC.

Note:
More detailed information on transferring the STEP 7 project to the WinAC is available in Entry ID: 18602609.

Configuring the SIMATIC HMI station for the Windows-based panel

  • Insert a SIMATIC HMI station via Insert > Station.

Fig. 4: Inserting a SIMATIC HMI station

  • Select the appropriate operator panel.

Fig. 5: Selecting the operator panel

  • Open the configuration of the SIMATIC HMI station.

Fig. 6: Configuration of the HMI station

  • Network the interface "HMI MPI/DP" with the PROFIBUS subnetwork of the WinLC.

Fig. 7: Networking HMI MPI/DP

  • Save and close the configuration.
  • Navigate in the SIMATIC Manager via the SIMATIC HMI STATION to WinCC flexible RT > Communications > Connections and double-click Connections in the right-hand project window. WinCC flexible 2004 opens.
  • Enable the displayed connection between the Windows-based operator panel and the WinLC.

Fig. 8: Enabling the connection in WinCC flexible 2004 ( 92 KB )  

  • You can then continue to configure the Windows-based operator panel in WinCC flexible 2004 (variables, pictures, messages ...).

 Entry ID:19550739   Date:2004-10-08