show the entry list
PROFINET general -- Product information -- System description
Where can you find information about the configuration and calculation of RCoax systems?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring the end-to-end link of 2x2 PROFINET cables?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
How can you implement the the communication concept of PROFINET CBA with PROFINET IO?
Why is hardware support required for using clock-synchronized real-time communication (IRT) in PROFINET?
How is to possible to transmit real-time messages at the same time as TCP/IP communication in PROFINET?
How can real-time communication (RT) be used with standard Ethernet hardware?
What should you watch out for when reconfiguring in RUN (CiR) if the configuration contains CiR elements and a PROFINET IO system?
Which settings have to be made on the Fluke DTX-1800 cable analyzer for testing cables in a PROFINET network?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
PROFIBUS general -- Product information -- System description
Which PROFIBUS connectors can you use in Zone 1 or 2?
Start-up characteristics of DP configuration after power supply OFF/ON
Parameter DP Master System ID
Failure of a master in a multimaster system
PRB checker with the Windows language setting German (Switzerland) 
Sporadic bus error with SIMATIC OPs on distributed I/O under S5 masters
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
Using S7 Communication, MPI, FDL or FMS on a PROFIBUS master system with Power Rail Booster
Changing from EN50170 to DPV1
Which products can you use with an RS 485-IS segment?
What options exist for using the BT200 tester on the PROFIBUS?
Which terminology do you use for cyclic PROFIdrive communication?
Which manuals are available to download from Industry Online Support regarding the diagnostic repeater and the RS 485 repeater?
Communication between two IM151 CPUs
How can you print on just one page the network topology determined via the Diagnostics Repeater?
Transferring the registration key to another PC/PG
Comparison of PROFINET and PROFIBUS
Part number:


QUESTION:
 
Is there an overview of the comparison between PROFINET and PROFIBUS?

ANSWER:  
As an introduction to PROFINET there is the PROFINET System Description (Entry-ID: 19292127) and the document PROFINET IO from PROFIBUS DP to PROFINET IO (Entry-ID: 19289930). These documents deal with the comparison of the communications technology and the necessary changes in the user program. This is due to the quantity structure that is partly enlarged in PROFINET IO.

The new blocks and system state lists (SSL) replace the previous versions and are for the most part compatible. They can be used equally well for PROFINET IO and PROFIBUS DP.

If you are only using PROFIBUS DP, in principle you can continue to use the usual blocks and system state lists for PROFIBUS DP. But it is recommended to switch to the new system and default functions in any case.


 Entry ID:19548537   Date:2004-10-05 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour