Description You can operate an ET200 CPU or an S7 CPU as PROFINET I device (intelligent IO device). The following holds here:
- An S7-300 CPU can be used as an I device as from firmware version V3.2.0.
- An S7-400 CPU can be used as an I device as from firmware version V6.0.0.
- An ET200S or an ET200pro CPU can be used as an I device as from firmware version V3.2.0.
- You need at least STEP 7 V5.5 for the configuration.
Note More information about the PROFINET I-device function is available in the system manual "PROFINET, System Description" in the chapter entitled "I Device" in Entry ID 19292127.
|