show the entry list
TeleService/TS/PC Adapter -- Setting up and parameterizing hardware -- Configuring devices
How do you commission the TS Adapter IE Advanced using the Engineering Tool STEP 7 (TIA Portal) V12 SP1?
Which settings and parameters are required to create a gateway from GSM to ISDN with TeleService S7?
How do you parameterize the TS Adapter II / IE modems for Australia and New Zealand?
TeleService with ET200S (IM151-CPU) and TS Adapter
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
How is the TS Adapter IE parameterized for an EDI connection with the product PCAnywhere?
What should you watch out for when parameterizing the initialization string for a modem with TeleService?
How do you commission a GSM wireless modem of the type M20 Terminal with TeleService S7 V5.x?
How are remote monitoring and control performed with TeleService IE?
What are the options for using the TS Adapter IE as standard router?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you set the local modem after installing TeleService V6.1?
Is there a check list for implementing a PC adapter?
How do you commission the TS adapter V5.x with the GSM modules TC35 terminal and TC35i terminal?
Call-back feature of the TS adapter v.5.x
Connecting to the Network via Auxiliary System
Connecting to the Network via Auxiliary System
Part number:

QUESTION:  
What can I do if I am not able to connect to the telephone network via an auxiliary system with TeleService?

ANSWER:  
If you wish to dial into the telephone network via an auxiliary station with TeleService, you will possibly get a busy dial tone. Thus, the Modem does not dial out of the auxiliary system.

Remedy:
Please verify whether the modem parameter ATX3 is set. ATX3 should be used on telephone - auxiliaries systems in order to avoid the waiting time  for the dial tone.

The parameter dialog for the parameter ATX3 can be found via the Windows-System configuration (Fig 1):
Telephone and Modem options >  Modems: Properties > Tab: Advanced 

Fig. 1: Configuration of the parameters "ATX3"

In auxiliary systems, do not set the option "Wait for dial tone before dialling". Please check the setting  (Fig. 2):
Telephone and Modem options > Modems: Properties > Tab: Modem 

Fig. 2: The option "Wait for dial tone before dialling" must not be set

In the dialling rules the valid numbers to access an outside line for local- and long distance calls have to be entered (Fig. 3):
Telephone and Modem options > Dialling rules: Edit Location > General: Dialling rules

Fig. 3: Access an outside line for local- and long distance calls


 Entry ID:19543455   Date:2004-10-13