Instructions:
ProTool provides the menu items Edit > Languages >
Exporting and Importing. These functions can be used for
the language extensions resp. messages of the ProTool-projects.
When exporting a configured language you can select a target
language to which the existing text will be translated.
- If you select Excel-table (*.csv) as an export format, the
exported texts will be stored as CSV-Files.
Note:
Further information for the export of texts with ProTool in
CSV-Files can be found in entry-ID: 13532007.
- With the Language Support Tool , that is installed from STEP 7
V5.3, you can also select Excel-Work folder (*.xls) as export
format, that means that the exported texts will be stored as
XLS-Files.
The export-files consist of two columns and can be opened with
Microsoft Excel. In the first column texts that have already been
configured are located. In the second column the according texts
are to be inserted. If the language configuration is finished, the
files can again be imported in ProTool .
Note:
In the language configuration of the Excel-File, no Texts are to
be added or modified!
Procedure for the export and import of texts with Protool via
XLS-Files in the target language Chinese in Windows
2000.
- Retrofitting of the chinese language support in Windows
2000
Open the Regional Options in the system properties. Set
the check box Simplified Chinese in the tab General
in Language settings for the system .
Figure 1: Retrofitting of Simplified Chinese
Files from the Windows 2000-CD are retrofitted, after that
please conduct a restart of the PC.
Reopen the Language Settings. Click on the button
Select System Locale ... In the tab General mark
Chinese (PRC) as standard, so that Chinese texts can be
edited. Confirm with OK.
Figure 2: Defining Chinese as Standard
Files from the Windows 2000-CD are retrofitted, after that
please restart your PC.
- Adding the Chinese keyboard layout in
Win2000
Change to tab Input and click on Add in
Installed Input Locales...
Figure 3: Adding Keyboard Layout
In Add Input Locale choose the setting Chinese
(PRC) and in Keyboard layout/IME the entry IME
(Input Method Editor). Please confirm with
OK.
Figure 4: Select Input Locale
In the Keyboard setting of Windows 2000 select "Chinese". Click
on the taskbar in the lower right at the Chinese IME-Symbol. With
this IME the Chinese signs can be generated via the German
keyboard.
Figure 5: Changing the Keyboard Scheme to Chinese
- Export of texts with ProTool in XLS-Files
Open your project and select Edit > Languages... >
Export in the ProTool-Menu bar
Figure 6: Exporting - Languages
Set up a storage location (Path) and as format Excel-Work folder
(*.xls) for the files. Select "German" as source language and
"Chinese" as target language. Confirm with OK.
The XLS-Files are newly created.
Figure 7: Target Language Chinese
Open the XLS-Files with Microsoft Excel. Insert the Chinese
translations from the second column into the texts of the first
column. Save the changes in the files and close
it.
- Import of texts in XLS-Files with ProTool
Start the import of the files via Edit > Languages... >
Import in ProTool. Choose a storage location of the modified
XLS-Files and confirm with OK.
Figure 8: Importing Texts
The ProTool-project is now also available in
Chinese.
Procedure for the export and import of texts with ProTool via
XLS-Files in the target language Chinese in Windows XP.
- Retrofitting of the Chinese language support in Windows
XP
Open the Regional- and Language options in the control
panel. In the tab Languages at Supplemental language
support set the tab at Install files for East Asian
languages.
Figure 9: Installing Files for East Asian Languages
Click on Apply in the Regional and Language options.
Files from the WindowsXP CD are retrofitted, after that
please conduct a Restart of the PC.
Reopen the Regional and Language Options. Change into tab
Advanced. Select Chinese (PRC) as "language for
non-Unicode supporting programs", so that in ProTool Chinese
symbols can also be used. Click on Apply. Possibly files
from the Windows XP CD are retrofitted, restart the PC
afterwards.
Figure 10: Language Versions of Programs, not supported by
Unicode
- Adding the Chinese keyboard layout in Windows
XP
Change into tab Languages and click on Details, to
add an Input Language for Chinese Input Language click on button
Add...
Figure 11: Adding Keyboard Layout
Select the setting Chinese (PRC) in Input Language
and in the selection box Keyboard layout/IME the entry
Chinese (Simplified) - ShuangPin. Confirm with
OK.
Figure 12: Adding Input Language
Exit Regional- and Language settings
Select the entry keyboard layout Chinese (PRC) in Windows
XP. Therefore click on the Chinese IME-Symbol in the lower right of
the taskbar. With this IME-Symbol the Chinese symbols can be
created via entry by the German keyboard!
Figure 13: Changing the Keyboard Layout in Windows XP
- Export of texts with ProTool in XLS-Files
Open your project und select Edit > Languages... >
Export in the ProTool-Menu bar.
Figure 14: Exporting - Languages
Set up a storage location (Path) and as format Excel-Work folder
(*.xls) for the files. Select "German" as source language and
"Chinese" as target language. Confirm with OK.
The XLS-Files are newly created.
Fig. 15: Target Language Chinese
Open the XLS-Files with Microsoft Excel. Insert the Chinese
translations from the second column into the texts of the first
column. Save the changes in the files and close
it.
- Import of texts in XLS-Files with ProTool
Start the import of the files via Edit > Languages... >
Import in ProTool. Choose a storage location of the modified
XLS-Files and confirm with OK.
Pic 16: Importing Data
The ProTool-Project is now available in
Chinese.
|