show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
WinAC RTX -- Configuring and programming communication -- Configuring communication to S7
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Information about the topic of "Configuring communication with the S7"
Transfer of WinAC Configuration from STEP 7 Configuration PC to WinAC-PC via MPI
WinAC RTX F -- Configuring and programming communication -- Configuring communication to S7
Information about the topic of "Configuring communication with the S7"
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Transfer of WinAC Configuration from STEP 7 Configuration PC to WinAC-PC via MPI
WinAC Basis -- Configuring and programming communication -- Configuring communication to S7
Information about the topic of "Configuring communication with the S7"
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Transfer of WinAC Configuration from STEP 7 Configuration PC to WinAC-PC via MPI
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Part number:

Introduction:
This entry provides instructions for configuring the internal connection between a WinLC and WinCC flexible Runtime.

Contents:

  1. Requirements
  2. Configuration of WinLC and WinCC flexible RT
    2.1 Configuration in a SIMATIC HMI station
    2.2 Configuration in a SIMATIC PC station
  3. Configuration with WinCC flexible

1. Requirements

  • MS Windows 2000 Pro SP4 or MS Windows XP Pro as from SP1
  • WinAC Basis as from V4.0, WinAC RTX as from V4.0, WinAC Slot as from V3.3
  • WinCC flexible Advanced
  • WinCC flexible Runtime
  • STEP 7 as from V5.3
  • SIMATIC NET as from CD 11/2003

2. Configuration of WinLC and WinCC flexible RT
You can configure WinLC and WinCC flexible Runtime (WinAC) in the SIMATIC Manager both in a SIMATIC HMI station and in a SIMATIC PC station.

2.1 Configuration in a SIMATIC HMI station
The table below explains the procedure for configuring the WinLC and WinCC flexible RT in a SIMATIC HMI station.
 
No. Procedure
1 Create a STEP 7 project
  • Create a new STEP 7 project with the SIMATIC Manager.
  • Place a SIMATIC HMI station in the project with "Insert > Station".


Bild 01

2 Select the operator panel
  • Select the operator panel "WinCC flexible RT".


Bild 02

3 Open HW Config and add WinLC
  • Double-click on configuration to get to the hardware configuration for the HMI station.
  • The application WinCC flexible RT was automatically inserted into the HMI station rack in slot 3.
  • Add a WinLC to slot 2 from the hardware catalog "SIMATIC HMI station > Controller > WinLC".
  • Save and compile the configuration.


Bild 03

4 Start the Station Configuration Editor and set parameters
  • Start the Station Configuration Editor via the toolbar or the icon on the desktop (SIMATIC NET must be installed).
  • With "Add...", you place a WinCC flexible RT and a WinLC on the same slots as in the hardware configuration (here: WinCC flexible RT slot 3 and WinLC slot 2).


Bild 04

5 Copy the station name
  • Copy the station name from the Station Configuration Editor and then use it to name the HMI station in the SIMATIC Manager.


Bild 05

6 Activate the "S7RTM is installed" option
  • Right-click on the SIMATIC HMI station in the STEP 7 Manager to open the "Object properties...".
  • Switch to the "Configuration" tab and activate the option "S7RTM is installed".
  • Close the "SIMATIC HMI station" dialog window.


Bild 06

7 Parameterize the PG/PC interface
  • Open the "PG/PC interface" in the menu "Tools > Set PG/PC interface" of the STEP 7 Manager.
  • Set the access point to "S7ONLINE (STEP 7) -->  PC internal (local)".


Bild 07

8 Start the WinLC Controller
  • Start the WinLC Controller.


Bild 08

9 Transfer the hardware configuration
  • Change to the hardware configuration of the HMI station again and load it via "PLC > Download to Module".
  • Close the hardware configuration of the HMI station.

2.2 Configuration in a SIMATIC PC station
The table below explains the procedure for configuring the WinLC and WinCC flexible RT in a SIMATIC PC station.
 

No.

Procedure
1 Create a STEP 7 project
  • Create a new STEP 7 project with the SIMATIC Manager.
  • Place a SIMATIC PC station in the project with "Insert > Station".


Bild 09

2 Select the operator panel
  • Double-click on Configuration to get to the hardware configuration for the PC station.
  • Add a WinLC to slot 2 from the hardware catalog "SIMATIC PC Station > Controller > WinLC" and a "WinCC flexible RT" application to slot 3 from the hardware catalog "SIMATIC PC Station > HMI".


Bild 10

3

Open HW Config and add WinLC
  • Save and compile the configuration.
  • Start the Station Configuration Editor via the toolbar or the icon on the desktop.
  • With "Add...", add a WinCC flexible RT and a WinLC to the same slots as in the hardware configuration (here: WinCC flexible RT to slot 3 and WinLC to slot 2).


Bild 11

4 Start the Station Configuration Editor and set parameters
  • Copy the station name from the Station Configuration Editor and then use it to name the PC station in the SIMATIC Manager.


Bild 12

5 Parameterize the PG/PC interface
  • Open the "PG/PC interface" in the menu "Tools > Set PG/PC interface" of the STEP 7 Manager.
  • Set the access point to "S7ONLINE (STEP 7) -->  PC internal (local)".


Bild 13

6 Start the WinLC Controller
  • Start the WinLC Controller.


Bild 14

7 Transfer the hardware configuration
  • Change into the hardware configuration of the PC station again and load it via "PLC > Download to Module".
  • Close the hardware configuration of the PC station.

3. Configuration with WinCC flexible
 
No. Procedure
1 Open WinCC flexible  
  • Navigate in the SIMATIC Manager via the SIMATIC HMI STATION or SIMATIC PC STATION to "WinCC flexible RT > Communication > Connections" and double-click in the right-hand project window on "Connections".

    => WinCC flexible opens.


Bild 15

2 Activate the connection
  • Activate the connection displayed between WinCC flexible RT and the WinLC via SOFTBUS.

    Note:
    Alternatively you can also activate the connection at Runtime with the system function "SetConnectionMode".


Bild 16

You can then continue with additional configuration (tags, pictures, messages etc.) in WinCC.

 Entry ID:19541601   Date:2010-03-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour