show the entry list
S7-200 PC Access and other OPC clients -- Configuring and programming communication -- Programming and connecting OPC clients
How can you access an S7-1200 PLC by PC Access and what is to be considered?
SIMATIC S7-200 -- How do you avoid the message "Not enough memory." in Excel diagrams in the case of data read out with PC Access?
How can you read data from the S7-200 CPU via the OPC client Excel with the OPC server PC Access and archive it in an Access database?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
How do you address variables areas of the SIMATIC S7-200 CPU via the SIMATIC NET OPC Scout?
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to PCs
Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML?
Which ports are used by WinCC flexible?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How do you integrate an HMI operator panel into a local network?
What options are there in WinCC flexible for using a Multi Panel or Mobile Panel as an OPC server?
What options are there in WinCC flexible 2004 for using a multipanel as an OPC server?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
Part number:


Instructions:

Software requirements:

  • S7-200 PC Access OPC Server V1.0.0.56
  • WinCC flexible 2004 Advanced
  • WinCC flexible 2004 Runtime

Hardware requirements:

  • S7-200 communications cable
  • S7-22x CPU
  • PC

A further requirement is that a properly functioning STEP 7 Micro/WIN project is available and loaded into S7-200 CPU.

Configuring the OPC server with S7-200 PC Access

  • Start S7-200 PC Access via Start > SIMATIC > S7-200 PC Access V1.0.0.56 > S7-200 PC Access.
  • Create a new project.


Fig. 01

  • Mark controller, e.g. "MicroWIN (CP5611(PPI))", and open the dialog Status > PG/PC Interface....
  • As access point of the application you must set "Micro/WIN" with the existing communications connection to the S7-200, e.g. "-->CP5611(PPI)".

Note:
If the access point is not "Micro/WIN", first close the dialog and set the access point via Control Panel > Set PG/PC Interface.

  • Close the dialog via OK.


Fig. 02

  • Via File > Import Symbols you import the symbol of the selected STEP 7 Micro/WIN project.
  • Then save the configuration you have created.
  • In S7-200 PC Access you can now access the symbol of the STEP 7 Micro/WIN project.


Fig. 03

  • If you mark the project folder "Project1", for example, you can check the address of the PLC via Edit > Properties.


Fig. 04

Checking the connection with Test OPC Client of S7-200 PC Access

  • Mark the symbols in the right-hand project pane of S7-200 PC Access.
  • Using drag and drop add the marked variables as items to Test Client (bottom project pane).


Fig. 05

  • Enable Test Client via Status > Start Test Client.
  • If "Good" is displayed for Quality, the variable has been read successfully out of the S7-200 controller.


Fig. 06

WinCC flexible Runtime as OPC client

  • Start WinCC flexible 2004 Advanced.
  • Create a WinCC flexible project for a PC via PC > WinCC flexible RT.
  • In the project tree double-click on Communication > Connections to create a new connection.
  • As communications driver for the connection select OPC.
  • Select "S7200.OPCServer" for OPC server.

Note:
If the S7-200 OPC server has not been started on the local PC, you must specify the computer name or the IP address of the remote PC on which the S7-200 OPC server is located. When accessing the OPC server via network, please refer to the DCOM settings in the WinCC flexible Online Help under "Communication > OPC > Commissioning the OPC > DCOM".


Fig. 07

  • Add a variable under Communication > Variables.
  • Via Symbol you select the relevant item of the S7-200 OPC server.


Fig. 08

  • You can display this variable via an input/output field in the Start picture.
  • Save the configuration.
  • Start WinCC flexible Runtime via the icon in the toolbar.


Fig. 09 


Fig. 10

 Entry ID:19514638   Date:2005-06-02