|
QUESTION:
What settings do I have to make to be able to practice
teleprogramming with STEP 5 via Industrial Ethernet?
ANSWER:
You wish to practice teleprogramming in STEP 5 via Industrial
Ethernet (ISO Industrial Ethernet, TC/IPA protocol).
You must meet the following requirements for ISO Industrial
Ethernet:
- Your PC must have a network card that is known to the operating
system.
- The "Softnet IE PG" software from the SIMATIC NET CD must be
installed.
- Set the "Siemens ISO Industrial Ethernet" protocol in
the network settings.
Windows 9x:
The "ISO Industrial Ethernet" protocol is located in the network
settings under "Protocols" at "Siemens AG".
Windows NT:
The "Siemens ISO Industrial Ethernet" protocol is in the network
settings of your computer.
Windows 2000 or Windows XP:
The protocol has already been installed with SIMATIC NET CD
7/2001 or 11/2002 and does not have to be installed again.
- Open the Control Panel via "Start >Settings > Control
Panel" and double-click the icon "Set PG/PC Interface".
- Set the access point "CP_H1_1:" to "ISO Industrial
Ethernet >Network Card". (Please do not forget to enter the
colon too!)
- Start STEP 5.
- In the STEP 5 menu "File > Project > Set", you can
now select the interface "Industrial Ethernet (Sinec
H1)".
If you are using Industrial Ethernet (TCP/IP), then the
same settings are valid for Windows NT as for ISO Industrial
Ethernet:
- Your PC must have a network card that is known to the operating
system.
- The "Softnet IE PG" software from the SIMATIC NET CD must be
installed.
- For implementing in Windows95/98 you need the additional
package "PG/OP Communication for CP1430 TCP" (only
necessary for TCP, not for TF modules).
This package is available as an option under order number
2XV9450-1AU04.
- Now add the "TCP/IP protocol" to the network settings of
your computer if the protocol is not yet available.
- Open the Control Panel via "Start > Settings > Control
Panel" and double-click the icon "Set PG/PC Interface".
- Set the access point "CP_H1_1:" to "TCP/IP
>Network Card". (Please do not forget to enter the
colon too!)
Fig. 1: Network properties in Windows 9x
- Restart your computer.
WARNING:
Points 7 to 9 apply only for Windows 9x. They are not
relevant if you are using Windows NT, Windows 2000 or
Windows XP.
- Start the "pgbus.exe" file from the "PG/OP Communication
for CP1430 TCP" additional package.
- The window that now opens shows that the TCP/IP driver is now
enabled.
Fig. 2: Message about enabled TCP/IP driver
- Now open the "snet_sw /S5_sw.bat" file from the
additional package. This starts STEP 5.
- Now start STEP 5 (only for Windows NT, Windows 2000 or
Windows XP).
- In the STEP 5 menu "File > Project > Set" you can
now select the interface "Industrial Ethernet (Sinec
H1)".
- With the bus path, please note that only an MAC address can be
specified. In this case you must convert the IP address into a
hexadecimal number and enter it into the first 4 bytes of the MAC
address (e.g. IP address: 140.80.0.20 is 8C.50.00.14.00.00 as MAC
address).
Einstellungen_STEP5.pdf ( 45 KB )
Warning:
No dial-up adapter may be installed, because then the the
interface "Industrial Ethernet (Sinec H1)" is not displayed in
STEP 5.
In Windows 9x please check in the menu "Start > Settings
> Control Panel > Network". If a Dial-up Adaptor is
displayed there, then please delete it.
Note:
If the access point "CP_H1_1:" is not in the PG/PC interface in
"Access Point of the Application", then you can add it
manually. Please specify the access point exactly as described in
Point 5.
|