QUESTION:
Which settings do I have to make in order to operate STEP 5
teleprogramming via PROFIBUS?
ANSWER:
The following requirements have to be met for teleprogramming in
STEP 5 via PROFIBUS. A distinction is made here between the
hardware platforms used:
- Computer with PCI slot(s)
- Computer with ISA slot(s)
- Laptop (Notebook or Field PG) with PCMCIA slot(s)
A. Using a computer with PCI slot(s)
- You need a CP 5613/5614 in your computer.
- Install the "CP5613/CP5614" software from the SIMATIC NET
CD.
- up to 05/2000: CP5613/CP5614 software V 2.1 (Windows NT
4.0/2000 Pro)
- as of 07/2001: CP5613/CP5614 software V 6.x (depending on SP of
Windows platform concerned)
- Open the Control Panel via Start > Settings > Control
Panel and double-click on the "Set PG/PC Interface"
icon.
Fig. 1: Selecting the access point
- Set the access point "CP_L2_1:" to "CP5613_5614
(PROFIBUS)".
- Start STEP 5. Open the Settings selection mask via File >
Project > Set in the PLC tab.
Fig. 2: STEP 5 selection mask "Set > Interface"
- Under "Interface" you select "PROFIBUS (Sinec L2)".
B. Using a computer with ISA slot(s)
- You need a CP 5412-A2 in your computer.
- Install the software "PG-5412" from the SIMATIC NET CD.
- Open the Control Panel via Start > Settings > Control
Panel and double-click on the "Set PG/PC Interface"
icon.
- Set the access point "CP_L2_1:" to "CP5412
(PROFIBUS)".
- Now start STEP 5.
- Under Settings you now select "Sinec L2
interface".
Warning: Make sure that the PROFIBUS parameters of
the network match those of the CP.
Note: If the access points are not available under
"Access Point of the Application" in the Set PG/PC Interface
window, then you can add them manually. Specify the access point
exactly as described in Point 4. Do not forget to specify the
colon.
C. Using a laptop (Notebook or Field PG) with PCMCIA
interface
A detailed description of the procedure for this is available in
Entry ID: 9831395.
|