|
QUESTION:
What settings do I have to make to be able to practice
teleprogramming with STEP 7 via Industrial Ethernet?
ANSWER:
You wish to practice teleprogramming in STEP 7 via Industrial
Ethernet (ISO Industrial Ethernet, TC/IP protocol). You must
meet the following requirements for ISO Industrial
Ethernet:
- Install a network card.
- Install the "Softnet IE S7" or "Softnet IE PG" software from
the SIMATIC NET CD.
- Now set the "ISO Industrial Ethernet" protocol in the
network settings.
Windows 9x:
The "ISO Industrial Ethernet" protocol is located in the network
settings under "Protocols" at "Siemens AG".
Windows NT:
The "Siemens ISO Industrial Ethernet" protocol is in the network
settings of your computer.
Note:
From SIMATIC NET CD 7/2001 no protocol installation is
required in Windows 2000 or Windows XP (from SIMATIC NET CD
11/2002).
- Open the Control Panel via "Start >Settings > Control
Panel" and double-click the icon "Set PG/PC Interface".
- Set the access point "S7(ONLINE)STEP7" to "ISO Industrial
Ethernet > Network Card".
- Start the SIMATIC Manager.
- Load your offline project via MPI into the controller and go
online by clicking the "Online" button in the SIMATIC Manager.
Note:
CPs of the *X11 series do not have to be loaded via MPI, because
they have been equipped ex works with a permanently set MAC
address. This then also provides a direct loading function via
Ethernet.
If you are using Industrial Ethernet (TCP/IP), then the
same settings are valid for Windows NT and Windows 9x as for ISO
Industrial Ethernet:
Note:
Here, too, from SIMATIC NET CD 7/2001 no protocol
installation is required in Windows 2000 or Windows XP (from
SIMATIC NET CD 11/2002), because this already be done to a great
extent by the operating system.
- Install a network card.
- Install the "Softnet IE S7" or "Softnet IE PG" software from
the SIMATIC NET CD.
- Now add the "TCP/IP protocol" to the network settings of
your computer if the protocol is not yet available.
- Open the Control Panel via "Start > Settings > Control
Panel" and double-click the icon "Set PG/PC Interface".
- Set the access point "S7ONLINE (STEP7)" to "TCP/IP->Network
Card".

Fig. 1: Setting the PG/PC interface
- Now start the SIMATIC Manager.
- Load your offline project via MPI into the controller and go
online by clicking the "Online" button in the SIMATIC Manager.
Note:
CPs of the *X11 series do not have to be loaded via MPI, because
they have been equipped ex works with a permanently set MAC
address. Here, since STEP 7 V5.1 SP 2, using the function "Assign
Ethernet Address" it is possible to assign an IP address via the
DLC protocol. This then also provides a direct loading function via
Ethernet.
Warning:
- In the case of older CPs, the Hardware Configuration
must be loaded into the controller via MPI.
- CPs of versions up to and including version EX10 can only be
addressed via your address after you have loaded the offline
project into the controller.
|