show the entry list
Industrial Ethernet S7-300/400 CPs -- Operation and maintenance -- Teleservicing
Teleprogramming via INDUSTRIAL ETHERNET with STEP 7
Which ports are used by the various services for data transfer by means of TCP and UDP and what should you watch out for when using routers and firewalls?
What requirements must be fulfilled and what should I watch out for when executing Routing?
What are the options for connecting a PG/PC online to the S7 controller via Ethernet?
What are the requirements for teleservice with STEP 7 in conjunction with a local ISDN card?
Industrial Ethernet PC CPs -- Operation and maintenance -- Teleservicing
Which ports are used by the various services for data transfer by means of TCP and UDP and what should you watch out for when using routers and firewalls?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
Alternative routes when setting up connections with the PG Channel Routing function
Teleprogramming via INDUSTRIAL ETHERNET with STEP 5 (PG BUS functions)
Teleprogramming via INDUSTRIAL ETHERNET with STEP 7
What requirements must be fulfilled and what should I watch out for when executing Routing?
Teleprogramming via INDUSTRIAL ETHERNET with STEP 7
Part number:

QUESTION:
What settings do I have to make to be able to practice teleprogramming with STEP 7 via Industrial Ethernet?

ANSWER:
You wish to practice teleprogramming in STEP 7 via Industrial Ethernet (ISO Industrial Ethernet, TC/IP protocol). You must meet the following requirements for ISO Industrial Ethernet:

  1. Install a network card.
  2. Install the "Softnet IE S7" or "Softnet IE PG" software from the SIMATIC NET CD.
  3. Now set the "ISO Industrial Ethernet" protocol in the network settings.
    Windows 9x:
    The "ISO Industrial Ethernet" protocol is located in the network settings under "Protocols" at "Siemens AG".
    Windows NT:
    The "Siemens ISO Industrial Ethernet" protocol is in the network settings of your computer.
    Note: 
    From SIMATIC NET CD 7/2001 no protocol installation is required in Windows 2000 or Windows XP (from SIMATIC NET CD 11/2002).
  4. Open the Control Panel via "Start >Settings > Control Panel" and double-click the icon "Set PG/PC Interface".
  5. Set the access point "S7(ONLINE)STEP7" to "ISO Industrial Ethernet > Network Card".
  6. Start the SIMATIC Manager.
  7. Load your offline project via MPI into the controller and go online by clicking the "Online" button in the SIMATIC Manager.
    Note: 
    CPs of the *X11 series do not have to be loaded via MPI, because they have been equipped ex works with a permanently set MAC address. This then also provides a direct loading function via Ethernet.

If you are using Industrial Ethernet (TCP/IP), then the same settings are valid for Windows NT and Windows 9x as for ISO Industrial Ethernet:
Note: 
Here, too, from SIMATIC NET CD 7/2001 no protocol installation is required in Windows 2000 or Windows XP (from SIMATIC NET CD 11/2002), because this already be done to a great extent by the operating system.

  1. Install a network card.
  2. Install the "Softnet IE S7" or "Softnet IE PG" software from the SIMATIC NET CD.
  3. Now add the "TCP/IP protocol" to the network settings of your computer if the protocol is not yet available.
  4. Open the Control Panel via "Start > Settings > Control Panel" and double-click the icon "Set PG/PC Interface".
  5. Set the access point "S7ONLINE (STEP7)" to "TCP/IP->Network Card".



Fig. 1: Setting the PG/PC interface

  1. Now start the SIMATIC Manager.
  2. Load your offline project via MPI into the controller and go online by clicking the "Online" button in the SIMATIC Manager.
    Note: 
    CPs of the *X11 series do not have to be loaded via MPI, because they have been equipped ex works with a permanently set MAC address. Here, since STEP 7 V5.1 SP 2, using the function "Assign Ethernet Address" it is possible to assign an IP address via the DLC protocol. This then also provides a direct loading function via Ethernet.

Warning:

  • In the case of older CPs, the Hardware Configuration must be loaded into the controller via MPI.
  • CPs of versions up to and including version EX10 can only be addressed via your address after you have loaded the offline project into the controller.

 Entry ID:1943727   Date:2003-03-21 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour