show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
Part number:

Description:
You have two S7 PLCs and one WinCC flexible Runtime station (PC station).
Data exchange between the WinCC flexible Runtime station and PLC station 01 is to be via MPI/DP and via Ethernet between the WinCC flexible Runtime station and PLC station 02.
When you try to create the two connections in WinCC flexible Runtime, the communication drivers are marked "orange".


Fig. 01

To achieve this task, you need one hardware interface for each access point (MPI/DP and Ethernet). 
One access point is created in the PG/PC interface for each of the two hardware interfaces. You can choose any name for the access points.

Instructions:
In this example, the first access point (MPI/DP) is named "S7ONLINE" and the second access point (Ethernet) "S7ONLINE_1".
 
No. Procedure
1 Creating and setting up a second access point:


Fig. 02

  • Call the PG/PC interface.
    "Start > Settings > Control Panel > Setting the PG/PC Interface".
    (Point 1)
  • Under "Access Point of the Application" you select <Add/Delete>.
    (Point 2)
  • Under "New Access Point:" you enter the name of the access point - in this example "S7ONLINE_1" - and press the "Add" button.(Point 3) Then close the window with the "Close" button.
  • In the "Set PG/PC Interface" window (Fig. 03), you select the parameter assignment used.
    In this example, "TCP/IP -> Your network card".
    Now, under "Access Point of the Application", you see the following name: "S7ONLINE_1  -->  TCP/IP -> Your network card".
    Close the window with the "OK" button.


Fig. 03

This completes setting up a second access point.

2 Defining the PROFIBUS connection:
  • Open the PG/PC interface with
    "Start > SIMATIC > STEP 7 > Set PG-PC Interface" or with "Tools > Set PG/PC Interface..." in the SIMATIC Manager.
  • There, under "Interface Parameter Assignment Used:" you select the CP you are using. In this example it is CP5512 (PROFIBUS).
    The access point of the application in this case is preset with
    "S7ONLINE   (STEP 7) -> CP5512(PROFIBUS)".
3 Parameterizing connections in WinCC flexible:
  • Open "Connections" in WinCC flexible.
  • Create a new connection for "PROFIBUS Communication".
    For "Access point" you use the default entry "S7ONLINE".
  • Create another connection for "Ethernet Communication".
    For "Access point" you do not use the default entry "S7ONLINE", but change it to "S7ONLINE_1".


Fig. 04

This completes parameterization of the connection in WinCC flexible.

4 Configuring a PC network:
Open the network connections with
"Start > Settings > Network Connections" and there you open the Properties of your network card.
Use the IP address that you defined in the WinCC flexible configuration.


Fig. 05

Keywords: 
Parallel communication

 Entry ID:19436008   Date:2008-07-11 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour