show the entry list
Industrial Ethernet network components (electrical/optical) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How to secure RUGGEDCOM ROS® Devices Before and After Field Deployment?
How do you incorporate the current version of your Scalance X 200 switch in STEP 7 through GSDML?
What options do you have for connecting an (R)STP segment to a ring structure and how can you reduce the ring reconfiguration time through the EPLC procedure?
What should you watch out for when configuring a Link Aggregation between SCALANCE X switches and RuggedCom switches?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via Industrial Ethernet and incorporating network components?
Which GSDML file can you use with the firmware version installed in SCALANCE X?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which settings have to be complied with in a PROFINET RT network in conjunction with VLAN switches?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
How do you transmit the diagnostics data of an OSM, ESM or SCALANCE to the TFTP server using the Trivial File Transfer Protocol (TFTP)?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Login window of the "Web Based Management" remains permanently active
What options do I have to insert a C-PLUG or what is the purpose of a C-PLUG?
Which Industrial Ethernet switches can be operated as redundancy managers and which as standby managers in a ring?
PROFIBUS network components (electrical/optical) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you set the DIP switches on the PROFIBUS OLM in order to achieve a line topology, a star topology or a redundant optical ring?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via PROFIBUS using S7 Communication and incorporating network components?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Network transitions and links (DP) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you parameterize IO Link master and devices across gateways with the S7 Port Configuration Tool (S7-PCT)?
How do you configure the DP/PA link in the external master / STEP 7 V12/V13 (TIA Portal)?
How do you link the AS-i Slaves to an S7-300 CPU with integrated PROFINET interface using the IE/AS-i Link?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via PROFIBUS using S7 Communication and incorporating an IE/PB Link gateway?
Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 using S7 communication and incorporating an IE/PB link gateway?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
How do you configure a ring redundancy with FDC 157-0 DP/PA couplers and active field distributors (AFDs)?
How do you connect a SIMATIC S7-300 as DP slave to a Y link in the hardware configuration of STEP 7?
Which options do you have for accessing PROFIBUS devices from a PC behind an IWLAN/PB link PN IO or an IE/PB link PN IO?
How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5? (GSD tool)
Incorporating new LINK modules in PCS7 V4.02
Set-up restrictions when using universal modules
Reduced user data capacity when using the diagnostics
Reading the input data of a DP slave configured by a different DP master
How do you configure an S7-300 CPU or a CP342-5 as DP slave to an S7-400H as DP master using a Y-link?
Configuration of the I/O Data on DP/DP Coupler
Retrieve Diagnostics of the DP/AS-i Link 20E
Configuring I/O addresses with DP/AS-i Link 20E
What are the special features of input/output addressing with the DP/DP coupler?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
Part number:

QUESTION:  
Is it possible to route data sets (PROFIBUS DP) and S7 via the IE/PB link gateway?

ANTWORT:  
The IE/PB link gateway - as an autonomous component- represents the seamless transition between Industrial Ethernet and PROFIBUS.

Besides PROFInet communication services, it additionally provides the subsequent functions:

  • S7 Routing
    S7 routing ensures PG/OP communication transcending networks. All S7 stations of PROFIBUS can be programmed from the distance from PG towards Industrial Ethernet. Moreover, data of S7 stations at the PROFIBUS can be accessed from panel stations (e.g. WinCC flexible RT) at the Industrial Ethernet.

Fig. 1: S7 Routing via IE/PB Link Gateway

  • Data Set Routing (PROFIBUS DP)
    The IE/PB link gateway can be used as router for data sets that are directed to field devices (DP slaves). Thus, PG/PCs that are not linked to PROFIBUS, and hence do not have a direct access on field devices are able to transfer data sets to field devices via IE/PB link gateway. E. g. by means of SIMATIC PDM on a PC at the Industrial Ethernet, you can parameterize and diagnose a  PROFIBUS via IE/PB link gateway.

Fig. 2: Data Set Routing via IE/PB Link Gateway

Note:
More information on IE/PB link gateway can be found in the manual "SIMATIC NET Net transition IE/PB Link Gateway" under Entry-ID: 7851748 or in the online help of STEP 7.


 Entry ID:19257092   Date:2004-07-28