show the entry list
HMI accessories -- Setting up and parameterizing hardware -- Using additional components
Why is the SIMATIC HMI SD Memory Card not recognized in a Comfort panel?
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Which hardware can be connected to the USB port of HMI operating devices?
Connecting two printers to a panel with serial interfaces
Mobile Panels -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Which can be connected directly to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Which hardware can be connected to the USB port of HMI operating devices?
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Machine Vision / Code reading systems -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you connect an MV320 hand-held barcode reader to an ET 200S and ET 200SP?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you perform a firmware update on an MV420/440?
How do you use Notepad++ to generate a match string message and transfer it with HyperTerminal?
Which hardware can be connected to the USB port of HMI operating devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the MV440 sensor to an S7-300 controller using ASM456?
How do you connect a SIMATIC HawkEye 4x(T) handheld code reading system to an ET 200S?
What should you watch out for when using a stationary code reading system with a hand-held lens in the immediate vicinity of a laser system?
What options do you have for connecting a handheld He4xT to a PC and what should you pay attention to here?
Which hardware can be connected to the USB port of HMI operating devices?
Part number:

Configuration Notes
You can connect the following devices to the USB port of HMI operating devices. For which panels have a USB interface, refer to Entry ID: 21847868.
 
Device Comments
Standard
USB mouse
-
Standard
USB keyboard
Note
The Windows CE operating system on the operator panels does not support German umlaut characters.
USB keyboard with trackball or touchpad The following operator panels were tested by way of example with both keyboards.
  • MP277
  • TP177B
  • Thin Client

Note
The Windows CE operating system on the operator panels does not support German umlaut characters.

USB stick See Entry ID: 21847868.
USB printer See Entry ID: 11376409.
Mobile hand-held barcode reader for 1D / 2D codes Recommended hand-held barcode readers
  • SIMATIC MV320
  • SIMATIC MV325
  • SIMATIC MV340

Please note, only use barcode readers which convert the barcode internally into an ASCII keyboard code.


Fig. 01

A detailed description of the devices is available in the relevant manuals in the following entry IDs.

  • SIMATIC MV320/ SIMATIC MV325 (Entry ID 78905254).
  • SIMATIC MV340 (Entry ID 61909865).
Industrial
USB Hub 4
The Industrial USB Hub 4 primarily serves as USB hub for the connection of peripheral devices to Panels, Multi Panels and Panel PCs with integrated USB interface. The simultaneous connection of up to four peripheral devices - such as USB stick, printer, keyboard, mouse, hand-held barcode reader - to one panel is possible with the Industrial USB Hub 4.


Fig. 02

Remark
Additional information about the Industrial USB Hub is available in the ST80 catalog and Entry ID: 23577105.

Important

  • The above recommendations do not reflect any official endorsement of equipment - except for the Industrial USB Hub 4. They simply represent a recommendation which is based on previous experience. In other words, responsibility for the use of these devices rests with you.
  • The current carrying capacity of the USB port differs depending on the type of operator panel. Refer to the relevant device manual in each case for precise specifications. It might therefore be necessary to provide an extra power supply for the device connected, for example, via the Industrial USB Hub 4.

Additional Keywords
USB devices, Trackball, Barcode scanner, Data Matrix Code, DMC

 Entry ID:19188460   Date:2014-03-13