show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Part number:

QUESTION:  
How do I assign the parameters of the ET 200S station if temperature compensation of a thermocouple is to be done by a resistance thermometer Pt100 for capturing the reference junction temperature?

ANSWER:  
The parameterization of both theIM151-1 (z.B. 6ES7 151-1AA03-0AB0) and the 2AI TC have to match each other.

  • 2AI TC: select "RTD" as reference junction and "1" as reference junction number.

In the parameters of the IM151 header station you have to activate the reference junction and specify the slot as well as the channel number of the Pt100 that captures the reference junction temperature.

Fig. 1: Operating parameters of IM151

In the parameters of the RTD module to which the Pt100 is connected for capturing the reference junction temperature you set, for example on channel 0 (Pt100 is connected to channel 0), the parameter "Type/range of measurement" to"RTD-4L Pt 100 climatic range".

Fig. 2: Parameters of the analog electronic module 2AI RTD

Fig. 3: Parameters of the analog electronic module 2AI TC

Notes:

  • More information on the possibilities regarding temperature compensation using thermo elements with ET 200S is available under Entry-ID: 19164525.
  • In contrast to IM151 (6ES7 151-1AA02-0AB0), the IM151 (6ES7 151-1AA03-0AB0) does not provide 8, but only 1 reference junction when using STEP 7 Version 5.3. Thus, the value "1" has to be set at parameter "Reference junction number" of the module 2AI TC ST. Spare parts are guaranteed, i. e. you will use IM 151 (...-1AA03-...) with the configuration of IM 151 (...-1AA02-...).


 Entry ID:19164641   Date:2004-08-23 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour