show the entry list
OS - WinCC -- Operation and maintenance -- Diagnosing errors
Why do you get the license error message "YMAINR9999 missing" although you are using only the license-free basic diagnostics?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How can you back up the data of the Windows event viewer?
How do you create a memory dump for diagnostics purposes in WinCC and PCS 7?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Why are the DCOM settings of the WinCC OPC server reset after activating the OS Runtime?
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why are the STEP 7 ActiveX controls (OCX) not shown on the OS server and OS client?
Why aren't all the block icons updated during OS compilation?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Why does the OS Login Box disappear sometimes in the background?
Length of mapped message texts
What should I do if the Split Screen Wizard closes with an error message?
Why do I get an error message when calling the loop display of a faceplate?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
What might be the cause that the hierarchy display in the overview area of the SIMATIC PCS 7 OS does not work?
Error Message "Group display: Tag .Eventstate does not exist"
Why does "?????" appear as a text on the range selector buttons in the overview area in OS runtime even though the text is available in the SIMATIC Manager?
Why does the error message 10111001 "The group display hierarchy has not been updated" appear?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
Part number:

Description
If the Basic Process Control (BPC) package is installed on a WinCC client in the WinCC network, the authorization check is made in a different way to when BPC is not installed. In this case BPC has to be installed on the server, because otherwise querying of the authorizations on the servers does not occur in the expected way and therefore the answer appears only after a certain delay.

Basic Process Control therefore either has to be installed on all the computers (server and clients) in a WinCC project or on none of them.

 Entry ID:19164182   Date:2011-07-08