QUESTION:
How do I parameterize the ET 200S, if the compensation of
temperature of a thermo element is intended to be done by the
reference junction inside the terminal module of the electronic
module 2AI TC HF (6ES7 134-4NB00-0AB0)?
ANSWER:
Especially designed for this task: module configuration with
terminal module TM-E15C24-AT (6ES7 193-4CL30-0AA0, spring-loaded
clamp) or TM-E15S24-AT (6ES7 193-4CL20-0AA0, screw clamp) and
the analog electronic module 2AI TC HF (6ES7
134-4NB00-0AB0).
The temperature values of the internal reference junction of
TM-E15C24-AT or TM-E15S24-AT only apply to this slot. Therefore
they are only available to the plugged electronic module 2 AI TC
HF.
For a correct configuration, the parameters of both the IM and
those of the module have to be set.
ET 200S Head Station
Regarding parameters of ET 200S head station IM151 (z.B. 6ES7
151-1AA03-0AB0) you should make sure to have the parameter
"reference junction" deactivated when using the
internal compensation of parameter "Reference junction".
Fig. 1: Parameters of IM 151
Analog Interface module
Please take the following settings into account when
parameterizing the analog electronic module 2AI TC HF:
- Generally, the parameter "Type/range of measurement" must show
value "deactivated" on unused channels.
- As reference junction, choose "RTD" for the corresponding
channel to which the thermo element is connected.
Fig. 2: Parameter of Electronic Module 2AI TC HF
Note: More information on possibilities regarding
temperature compensation using thermo elements on the ET 200S are
available under Entry-ID: 19164525.
|