show the entry list
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
Which can be connected directly to a panel?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Floppy disk drive on OP 15, OP 17 and C7-624
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Cable for loading the configuration onto OP/TP
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have?
Multi Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
Which can be connected directly to a panel?
What settings are to be made when connecting a printer to a Windows-based panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have?
Mobile Panels -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Which can be connected directly to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Which hardware can be connected to the USB port of HMI operating devices?
Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Part number:

Description
The document attached for downloading contains information on the topic of
USB transfer.

  • Tested USB cables
  • Released operator panels
  • Installation of the USB driver
  • Making a transfer to an operator panel via USB
  • Possible error messages and how to clear the errors

Note
Please bear in mind that over the course of time manufacturers/suppliers change their product or order designations, offer new versions of products or discontinue products from their range. Successor products are not necessarily suitable for transfer!

 Attachment 1: USB_Transfer_V1_0_e.pdf ( 726 KB )

Keywords
Project transfer, Transfer, USB driver, USB Master-Master, Lindy, 22408158

 Entry ID:19142034   Date:2011-08-19