|
Transfer options Attachment 1 lists the operator panels and their transfer options.
Attachment 1: Projecttransfer_V1_2_e.pdf ( 17 KB )
USB host-to-host cables
More information on the topic of "USB host-to-host cables" is available in Entry ID: 19142034.
Application of adapters and cables
Attachment 2 indicates for each operator panel the plug-in cable required for the following applications:
- Process coupling
- Download (update operating system, project, ...)
- Booting (filling in the case of a missing or damaged operating system)
Attachment 2: Panels_connecting_cables_V1_2_e.pdf ( 29 KB )
Notes on USB PC adapter (6ES7972-0CB20-0XA0)and USB A2 PC adapter (6GK1 571-0BA00-0AA0) The USB PC adapter/USB A2 PC adapter provides an MPI/DP interface through the PC's USB interface. More information about the USB PC adapter is available in the manual in Entry ID: 16983464 More information about the USB A2 PC adapter is available in the manual in Entry ID: 68849363 These cables are released only for the devices below for project transfer and OS updating.
- OP 73
- OP 77 A
- TP 177 A
- KTP600 Basic Color DP
- KTP1000 Basic Color DP
Using USB RS232 adapters and USB Ethernet adapters When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can only use the "real" interfaces for project transfer.
"Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters.
Additional Keywords Project transfer, Project download, WinCC flexible, Transfer cable, ProTool, RS 232, PC/PPI cable, PC PPI cable, RS 485, Com Text, Cables, USB adapter
|