show the entry list
WinCC (TIA Portal) -- Creating HMI configurations -- Loading and testing configurations
In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing?
What should you watch out for when downloading WinCC Runtime Professional from the Engineering Station to the Operator Station?
Why can you not transfer the HMI configuration to the panel?
Which connector cables are available for connecting to SIMATIC Panels?
Why does communication not work between WinCC Professional Runtime and S7-1200?
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
How do you configure the Autostart for WinCC Runtime Advanced V11 in Windows 7 Embedded?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
What do you have to do if you can no longer access symbols and data blocks of STEP 7 from an integrated WinCC flexible project?
Which entries are available on the internet for migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How do you save WinCC flexible projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
Which connector cables are available for connecting to SIMATIC Panels?
HMI accessories -- Setting up systems -- Transferring projects
Which connector cables are available for connecting to SIMATIC Panels?
C7 6xx -- Product information -- Background and system information
Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have?
The C7 6xx complete devices are to be discontinued in October 2010 – what are their successors?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How many connection resources can be managed by the C7-CPU or the C7-OP?
Which GSD file do you need for a C7 Complete Device?
Which software do you need for the C7-621 module (with integrated AS interface master)?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Overview of components integrated in a C7 complete system
Micro Panels -- Setting up systems -- Transferring projects
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Mobile Panels -- Setting up systems -- Transferring projects
In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing?
Why can you not transfer the HMI configuration to the panel?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Multi Panel -- Setting up systems -- Transferring projects
Why can you not transfer the HMI configuration to the panel?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Text display / Graphics devices -- Setting up and parameterizing hardware -- Setting up connections
Which connector cables are available for connecting to SIMATIC Panels?
Which GSD files are there for the Profibus DP operator panels?
Updating tags when a controller fails
What connecting cables are there for connections between the operator panels and the different controllers?
Testing the RS485 interface of a TD or OP
Basic Panels -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you integrate an HMI operator panel into a local network?
Which connector cables are available for connecting to SIMATIC Panels?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Pushbutton Panels -- Setting up and parameterizing hardware -- Setting up connections
Which connector cables are available for connecting to SIMATIC Panels?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Connecting PPs via PROFIBUS DP with the CP5431
Connection of a Pushbutton Panel to a S7-400H system via Y-Link
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
PP7 / PP17 with MPI on S7 200
S7-200 Operator Panels -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which connector cables are available for connecting to SIMATIC Panels?
To which extent can you incorporate a new TD 200(C) in a project that has been created with an older version of Micro/WIN?
TP070 - memory reset
Resetting the TD200C to the standard settings (standard menu and standard keyboard)
What should you watch out for when operating multiple TD100/200(C) text displays on a SIMATIC S7-200 CPU?
Under which circumstances can expansion modules or the TD 200 (C) lose their parameterization?
Comfort Panels -- Setting up systems -- Transferring projects
In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing?
Why can you not transfer the HMI configuration to the panel?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
Which connector cables are available for connecting to SIMATIC Panels?
Which connector cables are available for connecting to SIMATIC Panels?
Part number:

Detailed information on the topic of "possible connector cables for connecting to SIMATIC Panels" is available in the "ST 80 Catalog".

From the table in the "ST 80 Catalog" you can see which cable is supported by which panel and the function of the cable in each case.

Specifically, these are:

  • Cable that can be used for downloading (D)
    (operating system updating, project downloading, …).
  • Cable that can be used for the process connection (P).
  • Cable that can be used for an operating system update (U)
    (reset to factory settings).

The following figure shows an excerpt from this table.


Fig. 01

Go to the link below to download the "ST 80 Catalog" as PDF document.

To find the "ST 80 Catalog" faster use the "Filter" on the opened website. There you enter "ST 80".

In the "ST 80 Catalog" the information is in Chapter 2, in the section entitled "SIMATIC HMI Accessories - Connector cables".

More information on this topic

  • USB host-to-host cables
    Information on the topic of "USB host-to-host cables" is available in Entry ID: 19142034
  • USB PC adapter (6ES7972-0CB20-0XA0)
    The USB PC adapter provides an MPI/DP interface through the PC's USB interface.
    Information about the USB PC adapter is available in the manual in Entry ID: 16983464
  • USB PC adapter A2 (6GK1 571-0BA00-0AA0)
    The USB PC adapter A2 provides an MPI/DP interface through the PC's USB interface.
    Information about the USB PC adapter A2 is available in the manual in Entry ID: 68849363
  • The "USB PC adapter" and "USB PC adapter A2" are released only for the devices below for project transfer and OS updating. 
    • OP 73
    • OP 77 A
    • TP 177 A
    • KTP600 Basic Color DP
    • KTP1000 Basic Color DP
  • Using USB RS232 adapters and
    USB Ethernet adapters
    When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can use only the "real" interfaces for project transfer.
    "Real" interfaces are interfaces without prior implementation over USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters.

Additional Keywords
Project transfer, Project download, WinCC Advanced, WinCC Comfort, WinCC Basic, WinCC flexible, Connection cable, Transfer cable, ProTool, RS 232, PC/PPI cable, PC PPI cable, RS 485, Com Text, Cables, USB adapter

 Entry ID:19109408   Date:2013-09-18