show the entry list
S7-400 CPU 41x -- Product information -- Technical data
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Retentivity behavior of S7-400 CPUs and the CPU 318-2 CPUs
S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0)
S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0)
Part number:

QUESTION:  
What are the functions of the Operating Mode Switch of new CPUs (as of Firmware Version 4.0)?

ANSWER:  
New CPUs (Truncated Order No.: 6ES741x-xxx04-0AB0) are fitted with a toggle switch that has already been successfully in use with the S7-300 for some time. This toggle switch has three positions to select the current operating mode. The old key switch is void.


 
Old New
RUN-P RUN
RUN RUN + Protection Level 2
STOP STOP
MRES MRES

Tab. 1: Comparison of old and new functions of the Operating Mode Switch

Positions of the Operating Mode Switch

  • RUN (previously RUN-P) 
    The CPU processes the application program. In this case access to the periphery is possible. Programs can be retrieved with the PG from the CPU (CPU –> PG) as well as transferred into the CPU (PG –> CPU). Via protection level 2 (CPU configuration via HW Config)  the operating mode can be locked: merely read-only with blocks (previously RUN).

  • STOP 
    The CPU does not process an application program. Access to the peripherie is not possible. Programs can be retrieved with the PG from the CPU (CPU –> PG) as well as transferred into the CPU (PG –> CPU). 

  • MRES (Master Reset) 
    Position of the switch for the master reset of the CPU.

Note:
Cold start is further possible via STEP 7, but no longer via the operating mode switch.


 Entry ID:19065284   Date:2004-06-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour