show the entry list
WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtService (Teleservicing)
Why do you get an error message when opening the Sm@rtClient with the internet browser?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
What should you watch out with regard to licenses for WinCC flexible and panels?
What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)?
Connection to the SIMATIC WinCC flexible Sm@rtServer gets lost (with active screensaver or "Shut Down")
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Why do you get the message "Under Construction" in WinCC flexible when attempting to connect to the MiniWeb with the HTML viewer?
Why, when you call the Sm@rtClient, is only an empty page displayed in the Internet Explorer?
How do you send e-mails from a Windows CE panel or PC with SIMATIC WinCC flexible?
How do you send short messages (SMS) from an SIMATIC WinCC flexible HMI station to a mobile phone?
WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtAccess (Remote control)
How and where do you install access rights for the WinCC flexible options Sm@rtAccess and Sm@rtService?
What should you watch out with regard to licenses for WinCC flexible and panels?
What alternatives are there to the SOAP web service in Microsoft Windows Vista?
How do you temporarily lock multiple operator panels?
What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)?
How can you access tags of an operator panel using an Excel application with WinCC flexible 2008?
Connection to the SIMATIC WinCC flexible Sm@rtServer gets lost (with active screensaver or "Shut Down")
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Part number:

Description
The "Web Server" and "Remote" tabs are only in the "WinCC flexible Internet Settings" on a SIMATIC operator panel (only Windows CE devices) when a project is loaded with one of these options.

The "Web Server" tab is available when one of the following is checked in the project under "Device Settings > Runtime services":

  • Sm@rtService: HTML pages
  • Sm@rtAccess: Web service (SOAP)
  • Sm@rtAccess: SIMATIC HMI HTTP server

The "Remote" tab is available when the following is checked in the project under "Device Settings > Runtime services":

  • Sm@rtAccess or Service: Start Sm@rtServer


Fig. 01

If a project is transferred to the panel without one of the options mentioned above, the corresponding files are uninstalled and the tabs concerned are not displayed.

Note
The "E-mail" tab is independent of the project loaded and is thus always displayed.
Information on this is available in the corresponding manual for the panel at the following reference:
"Configure operating system > Configure network operation > Change e-mail settings".
For which devices support the Sm@rtAccess and Sm@rtService options see Entry ID 40227286.

Keywords
Setup, User interface, Menu, Tab, Internet settings, Configuration, SmartService, SmartAccess, SmartServer, Panel

 Entry ID:18982110   Date:2011-05-05