show the entry list
Industrial Ethernet S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you copy the CFC chart "Modbus" from the sample project for OPEN MODBUS / TCP into your user project?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
How is data with variable message length transferred via the TCP protocol and received by an S7-300 station via the Industrial Ethernet CP?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the UDP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol?
How do you program the FC10 "AG_CNTRL"?
Which commands (CMD) of the FC10 "AG_CNTRL" are supported by the IE CPs?
How many communication jobs may be used simultaneously in an S7-300 CPU for S7 communication via a CP343-1?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
Notes on using an instance for multiple connection IDs
Internal call of FC5 (AG_SEND) with FTP client blocks (FC 40-44) for the CP343-1 IT (6GK7 343-1GX11-0XE0)
How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
How do you program communication blocks FC11 and FC12 for the PROFINET IO device?
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
What should you pay attention to when using the communication blocks FC53 "AG_SSEND" and FC63 "AG_SRECV"?
What points do you need to remember when calling communication blocks FC5/50 and FC6/60 in the STEP 7 user program of the CPU?
How do you program communication blocks FC11 and FC12 for the PROFINET IO controller?
How can you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you program the communication blocks FC50 and FC60?
Error STATUS "0x7000" on function block FC6 / FC60 (AG_SEND) with Send/Receive communication on the S7-400 controller
How do you program the communication blocks FC5 and FC6?
Sample program: S7 communication with the blocks SFB14 ("GET") and SFB15 ("PUT") with S7-400
Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
"STATUS = 27" (0x001B) with the loadable S7 communication on the S7-300
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP
Part number:

QUESTION:  
How are the loadable communication blocks FB14 ("GET") and FB15 ("PUT") programmed for a data exchange on the S7-300 with a CPU 317-2PN/DP?

ANSWER:  
In order to exchange data between two S7-300 stations with a CPU 317-2PN/DP via a S7 connection which was configured with NetPro, in the S7 program communication blocks must be called. The block FB14 ("GET") serves to retrieve data out of a remote CPU and the block FB15 ("PUT") to write data into a remote CPU.

Properties of the Communication Block FB14 ("GET") and FB15 ("PUT") of the CPU 317-2PN/DP

  • FB14 and FB15 are asynchronous communication functions.
  • The blocks may run through several OB1 cycles.
  • FB14 or FB15 are activated via input parameter REQ.
  • The end of job is indicated by DONE, NDR or ERROR.
  • PUT and GET can communicate simultaneously via a connection.
  • The blocks are contained in a standard library of STEP 7 V5.3.

Attention:
You cannot use communication blocks of library SIMATIC_NET_CP for CPU317-2PN/DP.

The sample program contains a S7 connection via which data can be retrieved with a FB 14 from a remote CPU and data can be written with a FB15 into a remote CPU.

Description of the Sample Program

The STEP 7 project contains two stations S7-300 with CPU 317-2PN/DP for communication via Industrial Ethernet. A S7 connection was setup as the communications basis between both stations. In NetPro, if you open the properties of the S7 connection via "Right mouse click > Object properties", you can view the block parameter "ID" of the communication block. This information has to be taken into account, when calling FB14 or FB15, in order to facilitate a data exchange via a S7 connection.

  Fig. 1: Properties of the S7 Connection ( 53 KB )  

The STEP 7 program consists of blocks OB100, OB1, FB100, DB100, DB200, DB201, FB14 and FB15.

  • OB100
    OB100 is a start up OB and is executed during a reboot of the CPU (warm start). In this OB M1.0 and M0.1 release the first communication trigger.


Fig. 2: OB100 

  • OB1
    OB1 is called cyclically. In this OB the call of the FB100 (instance DB: DB100) is done with M1.0 and M0.1. After FB100 was executed, M1.0 is reset.


Fig. 3: OB1 

  • FB100
    FB100 is called in the OB1 cycle. In this FB you find the call of the FB14 ("GET") and FB15 ("PUT"). FB14 is activated via input parameter "REQ", if the interval marker M10.6 has a positive edge and no job is running.
    The input parameter ID must be adopted from the properties dialog of the S7 connection in NetPro (Fig.1). Parameter ADDR_1 contains that data area that is to be retrieved from a remote CPU. Parameter RD_1 contains the data area for retrieved data. Output parameters NDR, ERROR and STATUS are required for job evaluation and are only valid in the same cycle!


Fig. 4: FB100 - Invoking FB14

If the block was processed with error, the status word of the block is saved for error analysis.


Fig. 5: FB100 - Saving the Status Word

FB15 is activated via input parameter REQ, if clock memory M10.6 has a positive edge and no job is running. Input parameter ID must be adopted from the property dialog in NetPro (Fig.1). In case of parameter ADDR_1 the data area must be stated in the remote CPU, to which the values are to be written. With parameter SD_1 the address of the data to be sent is preset. Output parameters DONE, ERROR and STATUS are required for evaluating the job and are only valid in the same cycle!


Fig. 6: FB100- Invoking FB15

If block was processed with error, the status word of the block is saved for error analysis.


Fig. 7: FB100 - Saving the Status Word

STEP 7 Project as Download:
STEP 7 project contains a sample program on invoking the FB14 and the FB15 with status evaluation. It was designed with STEP 7 V5.3.

Cpu317-2_PUT_GET.exe ( 364 KB )  

Copy file "Cpu317-2_PUT_GET.exe" into a separate directory and then start the file with a double click. The STEP 7 Projekt will be automatically unpacked with all sub directories. You can now open and edit the project with SIMATIC Manager.

 Entry ID:18924842   Date:2004-05-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour