show the entry list
S7-300 CPU 31x -- Product information -- Technical data
How can you control the ALM (Active Line Module) of a CU320 (with DriveCLIQ) with the SIMATIC program?
Where can you find an update to use the SINAMICS with newer firmware in S7 Technology V4.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Why can't I see the values which are transmitted to an unlinked destination DB with SFC84, even though SFC84 is not indicating an error (RET_VAL = W#16#000?
How does the CPU 31x/31xC/C7 react when an MMC fault occurs during the save procedure?
What is the effect of the STEP 7 function "Copy RAM to ROM"?
Why does the SFC 54 "RD_DPARM" not work with the new S7-300 CPU with MMC?
How do you copy the user program from the load memory into the main memory without PG with a S7-300 CPU with MC slot?
How can you backup your program from the load memory?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
At which ambient temperature and at which air pressure can you operate a SIMATIC S7-300?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
S7-400 CPU 41x -- Product information -- Technical data
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Retentivity behavior of S7-400 CPUs and the CPU 318-2 CPUs
S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0)
ET 200S (standard modules) -- Product information -- Technical data
What are the requirements for using the S7 routing function and which modules can you implement?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which PROFIBUS connectors can you use in Zone 1 or 2?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates?
ET200S: How many motor starters can be allocated to a power module?
ET 200S: How many motor starters can be allocated to a power module?
ET 200S: How many load feeders may be connected?
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Baud rates for ET200S FO modules
Maximum power load for digital output modules
Minimum distance to the ET 200S front
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
WinAC RTX -- Product information -- System description
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which modules can you use when implementing software redundancy?
What are the requirements for using the S7 routing function and which modules can you implement?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Part number:

Description
The table below gives you an overview of the communication services that are supported by the CPUs with integrated PROFINET interface and by the WinAC RTX (F) via Industrial Ethernet.

18909487_CPUs_overview_e.pdf ( 16 KB )

The following entries include the manuals for the above-mentioned CPUs, which provide more information on the Technical Data, Communication Services and Quantity Frameworks.
 
CPU Entry ID
S7-300 12996906
S7-400 44444467
IM151-8 PN/DP CPU 47409312
IM154-8 CPU 44251850
WinAC RTX (F) 2010 43715176

The following entries give you an overview of the communication services that are supported by the S7-300 and S7-400 Industrial Ethernet CPs: Entry IDs  16767769 and 15368142.

Keywords
S7 communication, Open communication services, PROFINET IO, TCP, ISO-on-TCP, UDP, IO device, IO controller, PROFINET CBA

 Entry ID:18909487   Date:2011-08-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour