show the entry list
C7 6xx -- Setting up and parameterizing hardware -- Connecting and wiring modules
What options exist for ordering missing plug-in terminal strips for the power supply of panels?
C7-613: Power Supply of Digital Inputs
C7-633P: Suppressor Circuit of Current Inputs
C7-633P: Suppressor Circuit of Current Inputs
Part number:

QUESTION:  
How can I protect the current inputs of a C7-633P?

ANSWER:  
A suppressor circuit is sensible in the following cases, among others:

  • Wrong wiring of the input during the commissioning (e.g. 24 V are applied accidentally)
  • A fault of the sensor may cause e. g. a short circuit. Due to the damaged shunt resistor on the C7, the device would have to be sent in for repair.

Subsequent image shows a wiring diagramm, with which you can protect current inputs of a C7-633P.

Fig.1: Suppressor Circuit Analog Input ( 14 KB )  

Used Devices:
PTC: Company EPCOS, Order number B59980-C80-A70
Zenerdiode: Company Motorola, Order number 1N5339 (5,6V; 5W)


 Entry ID:18873380   Date:2004-04-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour