show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
Part number:

Description:
The ET 200S High Feature (header module IM151-1 HF) works by default as a DPV1 slave. The addresses in the header module cannot be packed with the default parameters.
To be able to pack the addresses with the ET 200S High Feature you must change the parameters of the header module.
You have two options.

  • Deactivate calling of OB 83 Insert/remove module interrupt or
  • Switch the DP Interrupt Mode to DPV0. This deactivates calling of OB 83.


Fig. 1: Switching off the Insert/remove module interrupt


Fig. 2: Switching over to DP Interrupt Mode DPV0

Note:
In Hardware Support Package, HSP0102 V1.4 onwards for the ET 200S interface module IM151-1 High Feature (6ES7 151-1BA02-0AB0), the Insert/remove module interrupt (OB 83) can be released even if there is a packed configuration present. For this you need firmware V2.2.1 for the interface module 6ES7 151-1BA02-0AB0.

You can install the Hardware Support Package in STEP 7 V5.3.2 onwards. Instructions for this are available in Entry ID: 17581199
The operating system update is available in Entry ID: 19728475

 Entry ID:18846664   Date:2008-02-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour