QUESTION:
How can I preset the maximum number of lines in the WinCC
Configuration Tool?
ANSWER:
The default maximum number of lines set in the WinCC Configuration
Tool is 2000.
WinCC_ConfigTool_01_en.gif)
Fig. 1: Default setting of the maximum number of lines
Proceed as follows to change this value:
Create a new WinCC project folder. Select "No connection".
WinCC_ConfigTool_02_en.gif)
Fig. 2: Creating a new WinCC project folder
Change the value of the maximum number of lines to the value you
require between 1000 and 65535, e.g. 15000.
WinCC_ConfigTool_03_en.gif)
Fig. 3: Changing the maximum number of lines to the required
value
Save the project folder.
Now, when you create a project map, the maximum number of lines
is set to the value you have just set in the procedure above.
|