show the entry list
Option PDM -- Working with projects -- Creating and editing projects
How do you use the different versions of SIMATIC PDM to access the devices that can be configured with SIMATIC PDM?
Loading Siprom projects
Transferring parameters from SIPART controllers on the SIPART DR net to SIPART controllers on the PROFIBUS DP net
Changing the address of a PA exchange device with SIMATIC PDM V5
Device assignment SIMATIC PDM up to V5.2
How can I incorporate ready-parameterized field devices from my Project A in a different Project B?
What are the requirements for using SIMATIC PDM Data Record Routing?
When is it possible to change a field device address?
How are HART field devices installed in the HW Config?
Why are there not any PDM devices available after you install SIMATIC PDM?
How do you use the HART secondary variables in addition to the actual HART process value in PCS 7?
How can I communicate with PDM (Process Device Manager) under Windows 2000 /XP Professional via the serial interface?
Working with Non-integrated Field Devices in SIMATIC PDM V5.1 through V5.2+SP1
Removing Devices in Network View in SIMATIC PCS 7 V6
How are PROFIBUS PA devices configured in PCS 7 V6.1 HW Config - and then in SIMATIC PDM V6.0 if the device first has to be imported into both configuration tools?
What should you do if devices which are imported subsequently are not displayed in the SIMATIC PDM device catalog (starting with PDM V6.0)?
What procedure should you follow if not all PA field devices are interconnected by the CFC driver wizard starting with PCS 7 V6.1?
How do you integrate devices into the SIMATIC PDM V6.0 at a later date?
Configuring field devices with SIMATIC PDM V5.2+SP1 and Hardware Configuration in PCS 7 V6.0
How do I configure and parameterize an ET 200iS with PCS 7 and PDM?
Removing Devices in Network View in SIMATIC PCS 7 V6
Part number:

QUESTION:  
I deleted devices in process device network view. Why do I still get the error message, "There is no authorization for the configuration of more than X devices..."?

ANSWER:  
The devices deleted from the network view are still in the process device plant view. The deletion from network view merely means that the assignment of the device to this network was removed. The device can then be assigned to another network. To completely remove the device, also delete the devices from the process device plant view.


 Entry ID:18778669   Date:2004-04-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour