Configuration Notes: There are revised function blocks
available for operating CP 342-5 (order number: 6GK7342-5DA02-0XE0)
or CP 342-5 FO (order number: 6GK7342-5DF00-0XE0). The following
table lists which functions you have to use.
|
FC type |
Version |
Can be used with module type CP 342-5
with order no. |
|
|
6GK7 342-5DA00-
0XE0 |
6GK7 342-5DA01-
0XE0 |
6GK7 342-5DA02-
0XE0 configured as ...DA00 or ...DA01 |
6GK7 342-5DA02-0XE0 / 6GK7 342-5DF00-0XE0 |
|
FC5 |
< V3.0 |
Yes |
Yes |
Yes |
No |
| FC6 |
< V3.0 |
Yes |
Yes |
Yes |
No |
| FC5 |
V 4.2 |
Yes 1) |
Yes 1) |
Yes |
Yes |
| FC6 |
V 4.7 |
Yes 1) |
Yes 1) |
Yes |
Yes |
| FC1 |
V 3.0 |
Yes 1) |
Yes 1) |
Yes |
Yes |
|
FC2 |
V 3.0 |
Yes 1) |
Yes 1) |
Yes |
Yes |
| FC1 |
V 1.11 |
Yes |
Yes |
Yes 1) |
No |
|
FC2 |
V 1.11 |
Yes |
Yes |
Yes 1) |
No |
|
1) |
Ignore temporary status = 80C4h (entry in diagnostics buffer:
"Error in miniprotocol") |
Warning: Please note that for these blocks byte is
the only permissible data type on the ANY pointer.
Keywords:
AG_SEND, AG_RECV, DP_SEND, DP_RECV
|