show the entry list
ET 200M (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Configuring SIPLUS extreme modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Which options are available for configuring the ET 200 stations?
Parameterization data of an analog module in an ET 200 are not transferred when using an external master
Configuring a power supply for an IMxxx in the ET200M
Configuring the Dummy Module => BF in ET200M
Parameterizing the ET200-M (IM153-x) only possible in hex code
The input values of an analog module in the ET 200M sporadically have the value zero
ET200-M with active backplane bus.
Configuring IM153-3 (ET200-M)
"Change of module during operation" parameter option on an ET 200 M
Operating ET200M as slave on master station CPU315-2DP
No startup of ET200M station when using blank slots
"Module change during operation" - Configuration and system requirements
Display of the "Parameter Assignment" tab for the configuration of modules
Output channels of SM 335 do not work
How do you calculate the times for the clock-synchronized operation of ET 200M?
"Change of module during operation" parameter option on an ET 200 M
Part number:

QUESTION:
What is the meaning of the "Change of module during operation" parameter option on an ET 200 M?

ANSWER:
Change of module during operation is a function with which certain modules from the S7 300 range can be removed from or plugged into the rack of the ET200M during operation.
However, the requirement here is that you have an active backplane bus (proper busbar with slots) and not the previous mounting channel with bus connectors.
Furthermore, you need at least an IM153-1AA02... or even newer.
Older modules like the IM153-0 or IM153-1AA00... do not support this function.
The IM 153 must be controlled by an S7-400 CPU, because the S7-300 CPU does not support the pull/plug interrupt.

As of Step7 V5.1 it will be possible for S7-300 to configure remove an plug, in particular when the CP 342-5 is used as DP master. Here you must remember that the connection to the CPU only functions via the FCs supplied. This means that an associated interrupt OB is not called. The remove/plug interrupt is also registered as a new diagnostic message of a module through the "DP-RECV" FC just like the other interrupts with this module. You must then read out the individual diagnostics of the slave and evaluate "manually" the sort of message concerned.

 Entry ID:186963   Date:2000-07-03 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour