show the entry list
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Connecting an S7-300 to a DP/PA-Link
Where can I procure the GSD files for my S7-300 CPUs?
Part number:

Description:
If you wish to connect a PROFIBUS DP slave, e.g. a CPU, to an external master, you need the GSD file. On an S7 master you can configure this directly via HW Config.
You can procure the GSD files for Siemens products directly via the Internet if the information is not in the module catalog of HW Config:

http://support.automation.siemens.com/WW/view/de/10805317/133100

You can reach the PROFIBUS GSD files: SIMATIC
in Entry ID 113652. The language is coded in the file designation, e.g. "xxxx.gse" stands for English. Please note how the order numbers of the CPUs, e.g. CPU 315, are assigned to the station types.

If you want to include the DP devices in the module catalog of HW Config, the GSD files must be stored on a data medium that you can access from STEP 7. How to do this is described in detail in Entry ID 2383630.

 Entry ID:186875   Date:2007-04-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour