show the entry list
Logon option -- Setting up development environments -- Parameterizing systems
How can you automatically log in a default user after a reboot without using the Login Box?
Using a chip card reader, how can a default user be logged on automatically while the chip card is pulled through?
Why isn't the user currently logged on shown at Runtime?
How can you verify a logged on user at runtime when using SIMATIC Logon (as from V1.3)?
How can you verify a logged on user at runtime when using SIMATIC Logon up to version V1.2 SP1?
How can you configure a chip card with SIMATIC Logon, with which you can log onto each local computer?
SIMATIC Logon window in CFC/SFC
How do you block a user account after a user-definable number of failed attempts to login?
How can you have entries generated by SIMATIC Logon in the password-protected file displayed, printed out or exported?
How can you restore the WinCC Logon Box in the OS Runtime when SIMATIC Logon is installed on the computer?
Why is a user assigned to the "Emergency Operator" group when logging on in WinCC RT?
When using SIMATIC Logon, why is there a user already logged on after starting WinCC RT?
Why, when implementing SIMATIC Logon, is only the logged-on user displayed in the WinCC User Administrator during Runtime?
Why does a C script "PWRTSilentLogin" only work with WinCC users and not with SIMATIC Logon users?
SIMATIC Logon window in CFC/SFC
Part number:

QUESTION:
How can I prevent the SIMATIC Logon window from appearing in CFC when I want to compile/download the S7 program?

ANSWER:
If you have installed SIMATIC Logon on your system, then all the activities that you run in CFC/SFC will be logged as well. For this you have to log in to the program with a user name and password each time you compile or download the program. To avoid this, in PCS 7 version V6.0 SP2 you can disable the Logon window and define a fixed user.

This fixed user is then logged on automatically for all PCS 7 applications from the time you start the SIMATIC Manager to the time you close the SIMATIC Manager. Please note that this automatic logon is valid for all PCS 7 applications, including some applications for which you might not wish to grant automatic access (e.g. OS, License Manager,...).

  1. In the SIMATIC Manager select Options > Simatic Logon Service.
  2. Enter the user name and associated password.

In the Start bar you now see the running SIMATIC Logon Service including the user logged on.


 Entry ID:18552666   Date:2004-03-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour