show the entry list
ES - SIMATIC Manager -- Working with projects -- Compiling OS and loading OS
What should you watch out for when downloading from the WinCC/PCS 7 Engineering Station to the Operator Station (ES-OS download)?
Why aren't all the block icons updated during OS compilation?
Which settings should you check if OS loading fails with PCS 7 or the OS project cannot be activated?
Problems when mapping data blocks with the same name
How can you clear the following error message during OS compilation: "The number of parameters for the structured DM variables xxx of type yyy does not match the number of operator-controlled connections...".
What is the meaning of the error message "A structure conflict occurred when creating the structured DM variable XXXX of type YYYY..." when compiling the OS?
How do you set the TCP/IP protocol for PLC-OS data transfer?
What is the meaning of the warning in the log file "*** Warning(s) ***: The structure type XXXX has been changed since the last compilation. All associated structured tags (even other S7 programs) will be deleted on the OS." ?
How do you use the template pictures "@PCS7Typicals*.pdl" to create block icons?
What does the compile OS error message "302:3018 - There are process variables whose names are not unique within the project after replacing special characters..." mean?
Which messages may appear in the "Download OS" dialog box?
Why appears the error message "The number of external DM variables in WinCC exceeds the permitted in total number", although the necessary license is available?
With PCS 7, why can't you open the OS project on the OS after it is downloaded from the ES?
Which special characters/separators may not be used in PCS7 V4, V5, and how are they replaced during AS/OS transfer?
What are the requirements for performing an online delta loading of the OS?
Why does the automatic package update of the clients sometimes not work in case of a changes-only download?
What do you do if a text which is configured in the CFC appears different in runtime?
How is a text, which has been configured in the CFC, transferred into the OS during OS compilation, and what do you have to watch out for in particular during configuration?
Which work steps are necessary for a project update of a redundant server couple and the MultiClients in SIMATIC PCS 7 V5.x?
Which work steps are necessary for the update of the OS Runtime data for the migration from PCS 7 V5.x to SIMATIC PCS 7 V6.x?
What do you do in PCS 7 V7.0 if the OS compile process is interrupted because the WinCC project cannot be opened?
Why can WinCC tags have the status "write-protected" and thus cannot be edited, deleted or moved?
What has to be watched out for during the compilation of a modification into the OS-Station after the interface modification of a Function block?
Why can't you transfer the elements of an S7 structure or UDT to WinCC through OS compilation?
Why doesn't OS delta load from the SIMATIC PCS 7 ES work despite Runtime being active on the OS station?
Why do you get a warning to the effect that your OS project is running in demo mode when testing it on your ES?
How can you clear the error message "Download (310:88)"?
How can you correct the error message "OS is currently being loaded from another ES"?
How is server data (server package) generated and loaded?
After reloading the OS project to the server from the ES, how do you clear the undefined error message and the abort?
When compiling the OS project, how can you clear the internal error 15500 in the transfer.log file?
Why does the error message "FileCopyError ....WinCC6.0_Project\GraCS\Default.pdd" occur when making a delta load and what is the "Default.pdd" file for?
Why are texts no longer updated with PCS 7 V6.0 SP3 + SP3 Postfixes after an OS delta compilation and OS delta load?
How do you clear the error message "*** Error(s) ***: Error while requesting messages from the STEP 7 message server...."?
How do you clear the error message "Internal error: transfer of process variables has been aborted. Error number: 15424" when compiling the OS project?
How can you clear the error message "No DM variable can be created for a symbol without a name" during OS compilation?
Why can't you load a project via a network?
Why do you get a warning to the effect that your OS project is running in demo mode when testing it on your ES?
Part number:

Description
You get this message if you are using PCS 7 options packages that are not licensed. This happens, for example, when using the "Redundancy" options package from PCS 7 OS, but do not have a license installed for it, or you have created a PCS 7 OS multi-user project, but have not installed a PCS 7 OS server license. You have the following options for avoiding this message.

  1. PCS 7 V4.x and V5.x
    In versions prior to PCS 7 V6.0 (V5.x, V4.x), no OS Runtime should be enabled on the ES as long as the redundant partner is entered in the redundancy properties. In these versions you should disable redundancy when testing the OS project on the ES. This is necessary, because the redundancy settings immediately become effective as soon as you activate/test the OS project. If you have a multi-user project, you will still get the message about the missing WinCC server license. Acknowledge this message or move it to the background so that you can continue testing on your ES.

    Warning 
    Reactivate redundancy after testing on the ES prior to transferring the OS project to the target station.

  2. PCS 7 V6.0 and newer
    In PCS 7 V6.0 and higher, you start simulation of the OS via SIMATIC Manager > Options > Start OS Simulation. Mark the OS to be simulated and start WinCC Runtime via "Start OS Simulation". With this call a copy of the OS project is automatically created for testing and redundancy is disabled prior to Runtime starting. If you have a multi-user project, you will still get the message about the missing WinCC server license. Acknowledge this message or move it to the background so that you can continue testing on your ES.

Note
More information on this topic is available in the PCS 7 Online Help under Getting Started PCS 7 - Part 2 > Preparations for Getting Started - Part 2 > Using a local PC station > How is a PC station used?.  

 

 Entry ID:18528943   Date:2010-09-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour